Skip to main content
STM.TestDev
Visitor II
Jan 6, 2023 6:16 AM UTC
Question

Cannot set DBANK=0 using v2.12.0 STM32CubeProgrammer. STM32G474

I'm trying to set the option bytes DBANK=0 thru CLI using v2.12.0 STM32CubeProgrammer

MCU: STM32G474

CLI argument: 

STM32_Programmer_CLI.exe -c port=SWD FREQ=1000 mode=UR LPM reset=HWrst -hardRst -e all -OB DBANK=0 -rst -e all -w C:\TestFW\TestHex.hex -v

Error:

PROGRAMMING OPTION BYTES AREA ...

Warning: Option Byte: dbank, value: 0x0, was not modified.

Warning: Option Bytes are unchanged, Data won't be downloaded

Time elapsed during option Bytes configuration: 00:00:00.015

While using the obsolete stlink utility 4.4.0, Option Bytes were updated successfully.

CLI Arguments:

ST-LINK_CLI.exe -c SWD FREQ=1000 UR LPM Hrst -ME -OB DBANK=0 -Rst -ME -P C:\TestFW\TestHex.hex -v after_programming

Success message:

Updating option bytes...

Option bytes updated successfully.

Just need to make this work on the STM32CubeProgrammer. Thanks

additional details

ST-LINK SN : 54FF6B066684565533271587

ST-LINK FW : V2J37S7

Board    : --

Voltage   : 2.60V

SWD freq  : 950 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x469

Revision ID : Rev X

Device name : STM32G47x/G48x

Flash size : 128 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xD5

This topic has been closed for replies.

1 reply

Ywang.3
Associate
Apr 20, 2023 10:02 AM UTC

Exactly, I have the same issue. I cannot use STM32_Programmer_CLI to set DBANK to be 0. Could someone tell us how to realize this? Thanks.