Skip to main content
SBint.1
Associate
Jun 8, 2022 4:06 AM UTC
Question

Cannot Open file in STM32CubeProgrammer

Before this all work fine until suddenly the file cannot be open. Tried to uninstall and delete all related file form pc then install back. Tried also to download the new and old version. The result in the same for both, still cannot open file. Can someone help me with this?

This topic has been closed for replies.

4 replies

ST Employee
Jun 8, 2022 7:11 AM UTC

Hi @SBint.1​ ,

I will try to help you on this issue ;) .

First let me clarify the situation, before that you was able to open your file with STM32CubeProgrammer and now that the issue is appeared a reinstall of STM32CubeProgrammer did not resolve the situation ?

  • Do you think the issue can be related to your file ? (may be the file is corrupted or damaged)
  • What's type of file do you want to open ? (.hex, .bin etc)

Thank you for your answers.

Best Regards,

A.MVE

SBint.1
SBint.1Author
Associate
Jun 8, 2022 7:23 AM UTC

True.

Before this problem happened, normally, after click the 'open file', the file explorer will appear, then suddenly, the file explorer does not appear that makes me unable to download the .hex file. I am not sure if this issue is related to the file or not.

ST Employee
Jun 9, 2022 7:14 AM UTC

Hi @SBint.1​ ,

I do not think that the issue is related to STM32CubeProgrammer either otherwise a reinstall or an upgrade of the application should solve your issue.

As the file explorer windows does not even appear after click on 'open file', I do no think that the issue is coming from the file. Maybe something on your computer block the right execution of STM32CubeProgrammer. Have you try to restart your computer ? Or any change you made on your computer (new software install, Anti Virus issue) ?

Best Regards,

A.MVE

Tesla DeLorean
Guru
Jun 8, 2022 9:16 AM UTC

Any details on file naming?

Is file on a networked drive or virtual directory?

Anti Virus blocking?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..