Skip to main content
TKamp.1
Associate
May 30, 2022 2:41 AM UTC
Question

Cannot install STM32CubeProgrammer 2.10.0 on os x 10.9.5

Hello everyone, I'm a beginner and want to try STM32 but there is a problem when installing STM32cube programming the message "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java".

I use :

osx :10.9.5

java version "1.8.0_331"

Java(TM) SE Runtime Environment (build 1.8.0_331-b09)

Java HotSpot(TM) 64-Bit Server VM (build 25.331-b09, mixed mode).

Thanks everyone hope someone can tell how to solve it.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jun 15, 2022 8:33 PM UTC

Hello @TKamp.1​ and welcome to the Community :)

Run STM32CubeProgrammer using admin rights.

There is no need to install any Java SE Run Time Environment since version 2.6.0.

The STM32CubeProgrammer runs with a bundled JRE available within the downloaded package and no longer with the one installed on your machine.

Please follow the UM2237 which describes the requirements and procedures to install the STM32CubeProgrammer software tool.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks