Skip to main content
JPark.20
Associate II
Sep 24, 2021 2:34 AM UTC
Question

can user dfu boot connection speed be as fast as the system boot?

hi!

i'm using stm32L4r9Ai.

​

i programmed user dfu boot (from 0x08000000 ~ 0x0800C000).

​

read, write, and erase operations are also performed normally in cubeprogrammer.

​

one problem is the speed at which the cube programmer connects to the device in the dfu boot state.

​

It is fast when connecting to a device in system memory boot state. It takes less than a second.

​

but, it takes about 6 seconds to connect to a device in the user dfu boot state. its too slow.

​

usb speed setting is the same in the image below.

​

0693W00000FAI7ZQAX.jpg <dfu boot connect>0693W00000FAI7eQAH.jpg <system memory boot connect> 

​

Is there a reason why the difference occurs and a way to solve this difference?

​

thanks!​

This topic has been closed for replies.