Skip to main content
Kabde
Associate
Sep 4, 2019 4:10 PM UTC
Question

Can't jump from bootloader to application on stm32l072cz that has cortex m0+

Hi,

I am writing a customized bootloader for STM32L072CZ (Cortex M0+) and I have an issue with performing the jumping from the bootloader to the application.

My application is linked at certain address (0x800b000) and I want to jump to this address from the bootloader. I've looked into a lot of online discussions but mainly for different stm32 processors.

Here is my code to do the jumping:

void mbed_start_application(uint32_t address) {

 __disable_irq();

 SysTick->CTRL = 0;

 // Disable IRQs & clear pending IRQs

 int i;

 for (i = 0; i < 8; i++) {

  NVIC->IP[i] = 0x00000000;

 }

 NVIC->ICER[0] = 0xFFFFFFFF;

 NVIC->ICPR[0] = 0xFFFFFFFF;

 // SCB->CPUID  - Read only CPU ID register

 SCB->ICSR |= SCB_ICSR_PENDSVCLR_Msk;

 SCB->VTOR = address;

 SCB->AIRCR = 0x05FA | 0x0000;

 SCB->SCR = 0x00000000;

 for (i = 0; i < 2; i++) {

    SCB->SHP[i] = 0x00;

 }

 SCB->SHCSR = 0x00000000;

 HAL_DeInit();

 /*GPIO_DeInit();

 HAL_RCC_DeInit();

 HAL_MPU_Disable();*/

 __set_MSP(*(__IO uint32_t*)address);

 /* Launch application */

 uint32_t JumpAddress = *(__IO uint32_t*)(address + 4u);

 pFunction Jump = (pFunction)JumpAddress;

 Jump();

}

Please point what I could be missing .

Thanks,

Khaled

This topic has been closed for replies.

4 replies

Uwe Bonnes
Chief
Sep 4, 2019 4:32 PM UTC

It is best to have a switch very early in the boot code before any initialization. That switch should look for a magic number in RAM that has not yet been initialized. If it sees the magic number, the number is reset and a jump to bootloader with setting Sysmen, vtor msp etc is done. User code , when boot loader is requested, sets that magic number and performs a warm reset.

Kabde
KabdeAuthor
Associate
Sep 4, 2019 4:50 PM UTC

Thanks for your answer Uwe but I would appreciate if you clarify what you mean. It's not clear for me what you mean by early switch and magic number in the RAM. Thanks!

Uwe Bonnes
Chief
Sep 4, 2019 5:00 PM UTC

Early in the boot code you test some RAM at known address for a know number (magic number). If the magic number is read, you branch (switch) to the code calling the system bootloader otherwise you proceed with your code.

Otherwise I do not see SYSCFG_CFGR1 set to 01. Maybe that is what is missing from your code.

Tesla DeLorean
Guru
Sep 4, 2019 5:12 PM UTC

Who will enable the interrupt you disabled?

What about the code on the app side using the correct vector table?

It is not jumping? Have you traced execution?

>>I've looked into a lot of online discussions but mainly for different stm32 processors.

The real problem is the shot-gun/kitchen-sink approach, and not really understanding the problem or the processor properly.

Or the interactions/expectations of the code on either side.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..