Skip to main content
Associate
May 27, 2024 7:32 AM UTC
Solved

Can't download the program!! :(

Hello, 

I want to download the program, STM32CubeProgrammer.

Before log in, download tap was visible and connectable.

However, After log in, download tap continues to load...

I've been waiting a long time, but it doesn't stop!!! :(

I also cleaned my cache data, but I can't see download tap.... 

I upload a captured picture..

 Please Help me... ㅠ^ㅠimege.PNG

This topic has been closed for replies.
Stassen.C
Stassen.CBest answer
ST Employee
May 27, 2024 12:27 PM UTC

Hi Inkong,

 

Can you try downloading on another browser? Or you can try to log out and download as guest also to see if it solves the issue.

Regards,
Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Stassen.C
Stassen.CBest answer
ST Employee
May 27, 2024 12:27 PM UTC

Hi Inkong,

 

Can you try downloading on another browser? Or you can try to log out and download as guest also to see if it solves the issue.

Regards,
Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
debugging
Lead
May 30, 2024 11:06 PM UTC

Cannot download. Using a ST account with  gmail account. Goes to page does not exist. . then selected a "guest" , it then says email is not validated. This is very very annoying ST !

Edit: got an email from ST with a link that worked. (hope the 'update" issues is now fixed as well ?

Explorer
Oct 21, 2024 5:39 PM UTC

Hello,

Got the same issue, still not resolved...