Skip to main content
Andrei Chichak
Lead
Jun 2, 2020 5:02 AM UTC
Question

Bug: STM32CubeProg 2.3.0 doesn't recognize S-record files.

In the Erasing & Programming tab the file path browse button dialog will not allow me to select an s-record file, even if the file type is s19, srec, or Srec.

Thanks.

This topic has been closed for replies.

2 replies

Nesrine.JLASSI
Visitor II
Oct 23, 2020 9:02 AM UTC

Hi @Andrei Chichak​ 

Please try with the last STM32CubeProgrammer version then tell me if it solve the issue.

Best regards,

Nesrine

Andrei Chichak
Lead
Oct 23, 2020 7:56 PM UTC

Yes, I see that 2.5.0 now understands .srec files.

ST's previous ventures DeFUse/DFU File Manager, and the Flash Loader Demonstrator chose to recognize the .s19 suffix instead of .srec. Is there any chance that your wizards could add .s19 as an alternative to .srec? Like recognize both?

Thanks,

Andrei