Skip to main content
FArdi.1
Associate II
Feb 14, 2024 3:09 AM UTC
Solved

BOR level description is confusing

Using latest STM32CubeProgrammer v2.15.0

Register name and description don't match (rising register, but falling description, and vice versa).

Which one is correct?

FArdi1_0-1707879998225.png

 

This topic has been closed for replies.
TDK
TDKBest answer
Feb 14, 2024 3:37 AM UTC

Rising voltage is higher than falling voltage. Description on the left is correct.

The reference manual is the best reference source.

TDK_0-1707881825148.png

 

 

See this post, STM32CubeProgrammer might be writing them to the wrong locations anyway. Unclear.

https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-2-10-0-released/m-p/134440/highlight/true#M1675

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

6 replies

TDK
TDKBest answer
Feb 14, 2024 3:37 AM UTC

Rising voltage is higher than falling voltage. Description on the left is correct.

The reference manual is the best reference source.

TDK_0-1707881825148.png

 

 

See this post, STM32CubeProgrammer might be writing them to the wrong locations anyway. Unclear.

https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-2-10-0-released/m-p/134440/highlight/true#M1675

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
FArdi.1
FArdi.1Author
Associate II
Feb 14, 2024 6:22 AM UTC

@TDK 

Thanks for the answer & the link to old issue.

At least for now the address location is correct for -ob BOR_EN=0x1 BORF_LEV=0x3 BORR_LEV=0x0

Only descriptions inside GUI need to be swapped.

FArdi1_0-1707891505342.png

FArdi1_1-1707891585986.png

 

 

TDK
Feb 14, 2024 2:52 PM UTC

Thanks for figuring that out and posting the result.

"If you feel a post has answered your question, please click ""Accept as Solution""."
FArdi.1
FArdi.1Author
Associate II
Mar 20, 2024 2:38 AM UTC

Description is unchanged with new v2.16.0. Still wrong, not match with Reference Manual.

But the release history said otherwise. See attached. 

KDJEM.1
ST Technical Moderator
Mar 21, 2025 11:57 AM UTC

Hello @FArdi.1,

 

Thank you for bringing this issue to our attention.

I reported internally.

Internal ticket number: 205883 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Jul 9, 2025 12:37 PM UTC

Hello @FArdi.1 ;

 

The issue is fixed in STM32CubeProgrammer 2.20.0 version.

 

Thank you.

Kaouthar 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.