Skip to main content
Associate
Sep 18, 2024 1:58 PM UTC
Question

Best/fastest API for C# desktop app read/write memory of several STM32 mcu's via StLinks, V2.1 and V3.

Currently I tried STM32Programmer_CLI and ST-LINK_CLI, both more than 100 times slower than StmStudio - StLink - SWD - MCU. The solution can only work up to 4Hz with 1 mcu and less with >1 mcu. StmStudio can run at least 250Hz with more exchanged data.

I tried this: "C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=SWD sn={serialNumber} mode=HOTPLUG speed=Fast -r8 0x20000000 0x8"

I need to run up to 20 mcu's simultaneously (6 is minimum), at least one must exchange data faster than 10Hz, prefer >50Hz, the rest can run 1Hz or sub 1Hz. Must be able to be addressed by StLink serialnumber.

Mcu firmware is locked so far. Mcu Hardware (circuit/PCB) is locked, so stuck with SWD, no USB/serialport.

Would another interface improve interface speed, e.g. Segger J-Link?

I am currently trying to get StLink-lib.dll working, will it be faster?

 

Please note, I am a hardware designer so software is not my primary job.

ANY advice is appreciated, especially if it is detailed and easy to understand, assume I am new to this.

Any guides/videos on this topic would be great, but any help/insight really.

 

This topic has been closed for replies.

10 replies

1234PJAuthor
Associate
Sep 18, 2024 2:16 PM UTC

This will be used for production tuning/testing of boards, minimum 6pcs and maximum 20pcs.

The solution I have tried so far has a high overhead, meaning it will open/close for each command/request and it contains much more data than what is relevant.

Best case, I can open "a channel" to a mcu, at this time all the "overhead" data is relevant, after that it would be beneficial if only SN of the stlink + the data was exchanged, I assume this is what stmstudio does?

Currently we are running a testsoftware in NodeRed/CobeMON, but it is very difficult to change from one testsoftware to another and it is not very stable.

I am not fixed on using C#.

Visitor II
Sep 18, 2024 2:20 PM UTC

Segger J-Link can provide a better speed. 

1234PJAuthor
Associate
Sep 18, 2024 2:22 PM UTC

Do you know how mush faster it is?

What would my approach be, I assume there might be more than one API available?

 

Andrew Neil
Super User
Sep 18, 2024 2:40 PM UTC

That would be specific to Segger - nothing to  do with ST.

Probably better to ask Segger: https://forum.segger.com/index.php/Board/3-J-Link-Flasher-related/

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Wasilewski.Piotr
Associate III
Dec 9, 2024 4:37 PM UTC

I'm using some high speed readout of ST-Link data in my MCUViewer software (It's like STMStudio, but actively maintained) - it's open source so maybe you can see how I've done it to get some inspiration :) JLink HSS mode is the fastest though (can reach tens of kHz with a few variables on JLink Ultra+).