Skip to main content
JBurg.5
Associate II
Jun 11, 2026 6:27 AM UTC
Question

Basic STM32 DFU Firmware Update Tool for End Users

Hello,

we manufacture products with STM32F7 MCUs. For firmware updates our customers use STM32CubeProgrammer via USB DFU mode. This is a robust and simple method. The only disadvantage of STM32CubeProgrammer is its complex functionality. Most of its features are useful for developers only. Is there a simplified GUI version without memory dump, option bytes menu etc., just for uploading a hex file?

 

Regards

Jan

1 reply

Michael E
ST Technical Moderator
Jun 11, 2026 6:48 AM UTC

Hello ​@JBurg.5 ,

A CLI is available with STM32CubeProgrammer tool. Help is available on UM2237 chapter 3.
It’s a solution to automatize or to simplify the tool.

Best regards

Michael

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.