Skip to main content
Associate
Mar 19, 2024 1:13 AM UTC
Question

ailed to connect STM32G431C8U6 via UART (Error: GETID command not acknowledged!)

Hello,

I'm trying to burn my program into the STM32G431C8U6 chip with UART on my PIN9 and PIN10.

When I want to connect the chip with STMCubeProgrammer and I got the following output:

08:57:10:466 : UR connection mode is defined with the HWrst reset mode
08:57:10:468 : RTS low
08:57:10:468 : DTR low
08:57:10:476 : Serial Port COM6 is successfully opened.
08:57:10:476 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
08:57:10:476 : No Init bits value is : 0
08:57:10:476 : Sending init command:
08:57:10:476 : byte 0x7F sent successfully to target
08:57:12:473 : Wait ends after 1 loop, dataready = 0, delay = 2000
08:57:12:474 : Timeout error occured while waiting for acknowledgement.
08:57:12:474 : No response from target received
08:57:12:475 : Retrying UART init connection...
08:57:12:477 : byte 0x7F sent successfully to target
08:57:12:483 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:12:483 : Received response from target: 0x1f
08:57:12:483 : Activating device: OK
08:57:12:483 : Board : --
08:57:12:483 : Sending GetID command and its XOR:
08:57:12:484 : byte 0x02 sent successfully to target
08:57:12:484 : byte 0xFD sent successfully to target
08:57:12:485 : Wait ends after 1 loop, dataready = 1, delay = 4
08:57:12:485 : Received response from target: 0x79
08:57:12:485 : Received 4 data bytes from target : 0x01046879
08:57:12:485 : Chip ID: 0x468
08:57:12:485 : Sending Get command and its XOR:
08:57:12:485 : byte 0x00 sent successfully to target
08:57:12:485 : byte 0xFF sent successfully to target
08:57:12:494 : Wait ends after 1 loop, dataready = 1, delay = 5
08:57:12:494 : Received response from target: 0x79
08:57:12:494 : Received 1 data bytes from target : 0x0b
08:57:12:495 : size of bytes in the response: 11
08:57:12:495 : Received 13 data bytes from target
08:57:12:495 : Full received response: 0b310001021121314463735072de
08:57:12:495 : BootLoader protocol version: 3.1
08:57:12:496 : byte 0x50 sent successfully to target
08:57:12:496 : byte 0xAF sent successfully to target
08:57:12:497 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:12:497 : Received response from target: 0x1f
08:57:12:497 : Response received from device: NACK
08:57:12:497 : byte 0x11 sent successfully to target
08:57:12:497 : byte 0xEE sent successfully to target
08:57:12:593 : data sent successfully to target: 0x0800000008
08:57:13:594 : Sending GetID command and its XOR:
08:57:13:596 : byte 0x02 sent successfully to target
08:57:13:596 : byte 0xFD sent successfully to target
08:57:13:602 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:13:602 : Received response from target: 0x1f
08:57:13:603 : Response received from device: NACK
08:57:13:603 : Error: GETID command not acknowledged!
08:57:13:699 : Reemission of GetID command
08:57:13:700 : Sending GetID command and its XOR:
08:57:13:703 : byte 0x02 sent successfully to target
08:57:13:705 : byte 0xFD sent successfully to target
08:57:13:712 : Wait ends after 1 loop, dataready = 1, delay = 4
08:57:13:712 : Received response from target: 0x79
08:57:13:712 : Received 4 data bytes from target : 0x01046879
08:57:13:714 : byte 0x11 sent successfully to target
08:57:13:714 : byte 0xEE sent successfully to target
08:57:13:811 : data sent successfully to target: 0x0800000008
08:57:14:810 : Sending GetID command and its XOR:
08:57:14:811 : byte 0x02 sent successfully to target
08:57:14:814 : byte 0xFD sent successfully to target
08:57:14:818 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:14:818 : Received response from target: 0x1f
08:57:14:818 : Response received from device: NACK
08:57:14:819 : Error: GETID command not acknowledged!
08:57:14:915 : Reemission of GetID command
08:57:14:916 : Sending GetID command and its XOR:
08:57:14:919 : byte 0x02 sent successfully to target
08:57:14:921 : byte 0xFD sent successfully to target
08:57:14:929 : Wait ends after 1 loop, dataready = 1, delay = 4
08:57:14:929 : Received response from target: 0x79
08:57:14:929 : Received 4 data bytes from target : 0x01046879
08:57:17:454 : Sending GetID command and its XOR:
08:57:17:454 : byte 0x02 sent successfully to target
08:57:17:455 : bytesToWrite before send = 1
08:57:17:455 : bFlushRet = 1, bytesToWrite after flush() = 1
08:57:17:455 : waitForBytesWritten Error : ??????????????? ????????
08:57:17:455 : byte 0xFD sent successfully to target
08:57:17:456 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:17:456 : Received response from target: 0x79
08:57:17:456 : Received 4 data bytes from target : 0x01046879
08:57:17:457 : byte 0x11 sent successfully to target
08:57:17:457 : byte 0xEE sent successfully to target
08:57:17:457 : data sent successfully to target: 0x0800000008
08:57:17:458 : UPLOADING OPTION BYTES DATA ...
08:57:17:459 : Bank : 0x00
08:57:17:459 : Address : 0x1fff7800
08:57:17:460 : Size : 44 Bytes
08:57:17:461 : Sending Read command and its XOR:
08:57:17:461 : byte 0x11 sent successfully to target
08:57:17:462 : byte 0xEE sent successfully to target
08:57:17:462 : Wait ends after 1 loop, dataready = 1, delay = 3
08:57:17:463 : Received response from target: 0x1f
08:57:17:463 : Response received from device: NACK
08:57:17:464 : Error: READ command not acknowledged at address: 0x1FFF7800
08:57:17:524 : Error: Uploading Option Bytes bank: 0 failed
08:57:17:571 : Error: Initializing the Option Bytes failed
08:57:17:641 : UART PORT CLOSE
08:57:17:642 : Disconnected from device.

 

I'm using a optoisolator then an USB toTTL converter to connect the PC and the board. I have checked several times the chip power supply the state of boot0 and the uart wiring. Do you have any ideas as to where the problem is?

Thanks

This topic has been closed for replies.

2 replies

ST Technical Moderator
Mar 19, 2024 5:04 AM UTC

Hello @Chanles and welcome to the Community :)

Which CubeProgrammer version are you using?

Are you making a reset in your application? Are you selecting "Run after programming"?

Could you please share the Option Bytes states?

Check this post, this may help you!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ChanlesAuthor
Associate
Mar 19, 2024 5:46 AM UTC

Hi Sir,

I'm using the version 2.15.0

Yes, I have the reset on my board and I tried but had the same result.

I dont select "Run after programming" cause it's a new chip and there's no program in it and I haven't been able to successfully connect and read the Option Bytes