Skip to main content
Associate
Jun 26, 2026 12:17 PM UTC
Question

"Uses FreeRTOS functions" from CubeMX1 not available in CubeMX2

In a project using FreeRTOS, we had the choice in STM32CubeMX to check a box in the NVIC panel “Uses FreeRTOS functions”, see here: 


I would love to have this feature available in STM32CubeMX2 as well, because by default the interrupt priorities are set to 0, and therefore need to be manually set to configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY (usually = 5) in order to use FreeRTOS API in those ISRs.

1 reply

Sara BEN HADJ YAHYA
ST Technical Moderator
Jul 20, 2026 1:15 PM UTC

Hello ​@TheBigBadBoy 

Thanks for your feedback, and I apologize for the late reply.

This request is currently under development. I will keep you posted and share any updates as soon as they are available.

Internal ticket number: CDM0064489 (This is an internal tracking number and is not accessible or usable by customers).

Regards,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.