Skip to main content
Associate II
Jul 10, 2026 1:55 PM UTC
Solved

USART1 receives garbage data at 1.5 Mbits/second or Higher (STM32C542RC)

Hi Team,

I am using the STM32C542RC on the STM32C5 Nucleo-64 board (MB2213),What is the max. supported baud rate for the USART baud rate?

We have checked that, with STM32CubeMX, the DIV1 prescaler, and oversampling by 16, the maximum supported USART baud rate is 9 Mbit/s, assuming the peripheral clock is configured appropriately.

However, in our setup, we are receiving garbage/corrupted data at 1.5 Mbit/s. Communication works correctly at 1 Mbit/s (TX and RX both working at this baud rate), but increasing the baud rate to 1.5 Mbit/s or higher in that case results in receiving garbage/invalid data.

 


The STM32 receiver and the sender are configured with the same UART settings:
Baud rate: 1.5 Mbit/s
Stop bits: 1 (also tested with 2)
Parity: None
Word length: 8 bits
Hardware flow control: None

 

Please check the above configuration and let us know how to achieve reliable data on the receiving end at a 1.5 Mbps or higher baud rate. If any additional configuration is required, then please let us know.

 

We need to support a higher baud rate with Tx and Rx both working, BUT due to this issue, we are not able to achieve that.

References

vatsalBest answer
Associate II
Aug 28, 2026 5:35 PM UTC

We were able to resolve this issue by enabling hardware flow control (UART 4-wire: TX, RX, RTS, CTS) between the STM32 and Jetson Orin Nano.

With hardware flow control enabled, we successfully achieved 1.5 Mbit/s communication with reliable TX/RX operation. We also successfully achieved 4 Mbit/s using the same approach.

The Clock Tree configuration remains based on HSE, and we also verified that both DMA- and interrupt-based communication work reliably at these baud rates.

This approach resolved the garbage/corrupted data issue we were experiencing at higher baud rates.

Thank you everyone for your support!

10 replies

Andrew Neil
Super User
Jul 10, 2026 2:09 PM UTC

What is the max. supported baud rate for the USART

The datasheet should tell you that?

 

Garbage data on async links is usually due to wrong baud rate - see here.

So the first thing to check is that the baud rate is really what you think it is.

Also use an oscilloscope to check that the signals are still valid at 1.5Mbps.

 

Please give some more details of your setup:

  • What is at the other end of the link ?
  • How are they connected ?

Some good, clear photos of your setup could help.

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
vatsalAuthor
Associate II
Jul 11, 2026 1:51 PM UTC

At the other end, Jetson Orin Nano Developer Kit Carrier Board is connected:
PIN 8: UART1_TXD     ↔     PB15: USART1_RX
PIN 10: UART1_RXD    ↔    PB14: USART1_TX
GND    ↔    GND

Jetson Orin Nano (Expansion Header Connections)

Commands:

1. Configure the UART:

stty -F /dev/ttyTHS1 1500000 cs8 -parenb -cstopb -crtscts -ixon -ixoff -ixany raw -echo

2. Send a message:

printf "hello world\n" > /dev/ttyTHS1


​​​Reference:

https://developer.nvidia.com/downloads/assets/embedded/secure/jetson/orin_nano/docs/jetson_orin_nano_devkit_carrier_board_specification_sp.pdf

 

 

 

MM..1
Super User
Jul 11, 2026 7:01 AM UTC

And ofcourse check if your clock tree is based on HSE and PLL is set right for 1,5Mb divider without error.

Andrew Neil
Super User
Jul 11, 2026 8:44 AM UTC

And ofcourse check if your clock tree is based on HSE 

Indeed.

 

​@vatsal using an internal RC oscillator is unlikely to give good baud rate accuracy - especially at such high speeds.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Gyessine
ST Technical Moderator
Jul 15, 2026 10:53 AM UTC

Hello ​@vatsal 

I’m quite confident that your issue is related to clock accuracy.

The USART has a maximum tolerance for clock frequency deviation. If this tolerance is exceeded, it can result in framing errors or garbled characters on the received data.

Could you please confirm which clock source you are using: HSI or HSE?

For high baud rates such as 1.5 Mbit/s, we strongly recommend using HSE, as it is typically much more accurate and stable than HSI.
Since HSI is less precise, it may cause the system clock to exceed the USART’s allowable tolerance.

You can also verify the clock accuracy using MCO, and calculate the allowed deviation based on the following section of the reference manual:

43.5.9 Tolerance of the USART receiver to clock deviation
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
unsigned_char_array
Lead III
Jul 15, 2026 12:02 PM UTC

For high baudrates I recommend using DMA for reception instead of interrupts.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
MM..1
Super User
Jul 15, 2026 3:36 PM UTC

Orin cant handle  

 stty -F /dev/ttyTHS1 1500000

result speed is not as you write, but what hw is capable. Here maybe baud = 68 000 000 / (16 × 3) = 1 416 666,7 baud

Set both sides to same speed .

ST Employee
Jul 21, 2026 3:33 PM UTC

Hello all, 

Likely not a USART1 max-rate limitation, but a baud-accuracy mismatch at higher speed.

1.5 Mbit/s can fail if either side’s real baud is off (even when configured the same), especially with HSI or rounded divisors on the peer side. Since 1 Mbit/s works and 1.5 Mbit/` corrupts, this points to timing margin, not feature support.

I’d check:
1. STM32 clock source: use HSE+PLL (avoid HSI for this case).
2. Actual baud on both sides with a scope/logic analyzer.
3. Jetson actual achievable divisor/rate for 1500000 and match both ends exactly.
4. Signal quality/wiring/ground at high edge rates.

If needed, switch to DMA RX once timing is fixed, but DMA won’t solve a baud mismatch by itself.

Kind regards, 

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"
vatsalAuthorBest answer
Associate II
Aug 28, 2026 5:35 PM UTC

We were able to resolve this issue by enabling hardware flow control (UART 4-wire: TX, RX, RTS, CTS) between the STM32 and Jetson Orin Nano.

With hardware flow control enabled, we successfully achieved 1.5 Mbit/s communication with reliable TX/RX operation. We also successfully achieved 4 Mbit/s using the same approach.

The Clock Tree configuration remains based on HSE, and we also verified that both DMA- and interrupt-based communication work reliably at these baud rates.

This approach resolved the garbage/corrupted data issue we were experiencing at higher baud rates.

Thank you everyone for your support!