Skip to main content
Associate
Nov 7, 2026 12:56 PM UTC
Question

STM32CubeMX2 v1.2.0 stuck in a restart loop and fails to load the project creation screen

 

I have removed version 1.0.1 from the /opt/st/ directory and installed the new version 1.2.0

I also updated my Debian Linux distro to the latest with apt full-update.

When the program is started I am presented with a Restart pop-up, clicking the Restart button will revert back to the same pop-up (endless loop).

After clicking Cancel in the pop-up it will unfortunally stm32cubemx2 just sit with a rotating thing on the Create application project from mcu screen.

 

Roelof

 

Moved from Cannot create a project with STM32CubeMX2

 

1 reply

Visitor
Nov 11, 2026 12:00 PM UTC

Had the same issue. Removed the `~/.theia-cubemx2/`directory solved the problem.