Skip to main content
Sara BEN HADJ YAHYA
ST Technical Moderator
Jul 7, 2026 5:59 PM UTC
StickySolved

STM32CubeMX2 v1.1.0 released

We’re happy to announce that STM32CubeMX2 v1.1.0 has been released and is now available.

 

This release includes updates and improvements aimed at enhancing the user experience and supporting your development workflow with STM32.

 

What’s new

  • Enhanced installation support for multiple STM32CubeMX2 versions, including linked IOC2 files and a pinned icon on the Windows taskbar
  • Added Expand All and Collapse All functions in software configuration panels
  • Added confirmation dialog boxes for selected actions
  • Added options to export the pinout as CSV from a menu: without alternate functions or with alternate functions
  • Added pin labels that can be used from configuration panels
  • Improved command-line interface (CLI) capabilities for software configuration
  • Added a pack version compatibility check
  • Added end-user guidance to run Pack update steps in the correct order, with a focus on device family pack (DFP) and hardware abstraction layer (HAL) packs
  • Increased pin name visibility in the pinout view to improve readability
  • Added the possibility to view all parts that compose a module allowing the end user to enable individual selection and more granular management
  • Improved consistency between clock tree source selection and reset and clock control (RCC) configuration
  • Improved overall performance and robustness
  • A script is now available to create STM32CubeMX2 projects using the STM32C5 v2.0.0 packs instead of the latest published pack version (refer to Workaround for creating STM32CubeMX2 projects with a non-latest pack version)

Get it here

Download STM32CubeMX2 from the ST Developer Zone.

Learn more

For full details, refer to the official STM32CubeMX2 documentation.

Release details

For the list of new features and major fixes, refer to Release details. 

A few limitations

For the list of known limitations, refer to Release limitations.

 

We encourage you to try the new version and share your feedback with us.  STM32CubeMX2 (MCUs) - STMicroelectronics Community 


The STM32CubeMX2 Team

This topic has been closed for replies.
Sara BEN HADJ YAHYA
ST Technical Moderator
Jul 7, 2026 6:00 PM UTC

This is an announcement post, if you have any issue or feedback to report please use the main page: STM32CubeMX2 (MCUs) - STMicroelectronics Community 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Sara BEN HADJ YAHYA
Sara BEN HADJ YAHYAAuthorBest answer
ST Technical Moderator
Jul 7, 2026 6:00 PM UTC

This is an announcement post, if you have any issue or feedback to report please use the main page: STM32CubeMX2 (MCUs) - STMicroelectronics Community 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.