Senior
Jun 17, 2026 3:15 PM UTC
Question
Incorrect DMA channel parameter
- 1 reply
- 114 views
Hello,
I have an application that set up TIM2 as a input capture timer that worked fine with HAL 2.0.0. After upgrading to HAL/template 2.1.0 I regenerated the code with MX2 but the code does not compile. The error occurs when compiling this line of code in LPDMA1_CH1_IRQHandler() mx_tim2.c:
HAL_DMA_IRQHandler(&hLPDMA1_CH1);A different DMA channel variable is defined earlier in the file and MX2 also displays LPDMA1_CH2 as the DMA used for TIM2.
static hal_dma_handle_t hLPDMA1_CH2;To make the code work I changed code in this file I had to replace LPDMA1_CH1 with LPDMA1_CH2 in several places in this file. Here is the new code:
/**
******************************************************************************
* @file : mx_tim2.c
* @brief : Peripheral initialization
******************************************************************************
* @attention
*
* Copyright (c) 2026 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the mx_stm32c5xx_hal_drivers_license.md file
* in the same directory as the generated code.
* If no mx_stm32c5xx_hal_drivers_license.md file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "mx_tim2.h"
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Private functions prototype------------------------------------------------*/
/* Exported variables by reference--------------------------------------------*/
static hal_tim_handle_t hTIM2;
static hal_dma_node_t DMA_Node_TIM2_CC4;
static hal_dma_handle_t hLPDMA1_CH2;
/* Exported function definition ----------------------------------------------*/
/******************************************************************************/
/* Exported functions for TIM2 in HAL layer */
/******************************************************************************/
hal_tim_handle_t *mx_tim2_init(void)
{
if (HAL_TIM_Init(&hTIM2, HAL_TIM2) != HAL_OK)
{
return NULL;
}
HAL_RCC_TIM2_EnableClock();
/* Timer configuration to reach the output frequency at 1 kHz */
hal_tim_config_t config;
config.prescaler = 143;
config.counter_mode = HAL_TIM_COUNTER_UP;
config.period = 0x3E7;
config.repetition_counter = 0;
config.clock_sel.clock_source = HAL_TIM_CLK_INTERNAL;
if (HAL_TIM_SetConfig(&hTIM2, &config) != HAL_OK)
{
return NULL;
}
/* Sampling Clock */
if (HAL_TIM_SetDTSPrescaler(&hTIM2, HAL_TIM_DTS_DIV1) != HAL_OK)
{
return NULL;
}
if (HAL_TIM_SetDTS2Prescaler(&hTIM2, HAL_TIM_DTS2_DIV1) != HAL_OK)
{
return NULL;
}
hal_tim_ic_channel_config_t ic_config;
ic_config.source = HAL_TIM_INPUT_TIM2_TI4_GPIO;
ic_config.polarity = HAL_TIM_IC_FALLING;
ic_config.filter = HAL_TIM_FDIV1;
if (HAL_TIM_IC_SetConfigChannel(&hTIM2, HAL_TIM_CHANNEL_4, &ic_config) != HAL_OK)
{
return NULL;
}
hal_tim_ic_capture_unit_config_t ic_capture_unit_config;
ic_capture_unit_config.source = HAL_TIM_IC_DIRECT;
ic_capture_unit_config.prescaler = HAL_TIM_IC_DIV1;
if (HAL_TIM_IC_SetConfigCaptureUnit(&hTIM2, HAL_TIM_IC_CAPTURE_UNIT_4, &ic_capture_unit_config) != HAL_OK)
{
return NULL;
}
/* Update Event Management */
if (HAL_TIM_SetUpdateSource(&hTIM2, HAL_TIM_UPDATE_REGULAR) != HAL_OK)
{
return NULL;
}
if (HAL_TIM_EnableUpdateGeneration(&hTIM2) != HAL_OK)
{
return NULL;
}
/* Master Mode Configuration */
/* Capture/Compare DMA request selection */
if (HAL_TIM_SetCaptureCompareDMAReqSource(&hTIM2, HAL_TIM_CC_DMAREQ_CC) != HAL_OK)
{
return NULL;
}
/* ### TIM2 GPIO Configuration ########################### */
/* GPIO Clocks activation */
HAL_RCC_GPIOC_EnableClock();
hal_gpio_config_t gpio_config;
/**
[GPIO Pin] ------> [Signal Name] ------> [Labels]
PC4 ------> TIM2_CH4 ------> PC4
**/
gpio_config.mode = HAL_GPIO_MODE_ALTERNATE;
gpio_config.output_type = HAL_GPIO_OUTPUT_PUSHPULL;
gpio_config.pull = HAL_GPIO_PULL_NO;
gpio_config.speed = HAL_GPIO_SPEED_FREQ_LOW;
gpio_config.alternate = HAL_GPIO_AF_1;
HAL_GPIO_Init(PC4_PORT, PC4_PIN, &gpio_config);
/* Enable the Timer global interrupt */
HAL_CORTEX_NVIC_SetPriority(TIM2_IRQn, HAL_CORTEX_NVIC_PREEMP_PRIORITY_5, HAL_CORTEX_NVIC_SUB_PRIORITY_0);
HAL_CORTEX_NVIC_EnableIRQ(TIM2_IRQn);
/* Timer Capture/Compare 4 DMA Request Configuration */
if (HAL_DMA_Init(&hLPDMA1_CH2, HAL_LPDMA1_CH2) != HAL_OK)
{
return NULL;
}
HAL_RCC_LPDMA1_EnableClock();
hal_dma_direct_xfer_config_t xfer_cfg_tim2_cc4_dma;
xfer_cfg_tim2_cc4_dma.request = HAL_LPDMA1_REQUEST_TIM2_CC4;
xfer_cfg_tim2_cc4_dma.direction = HAL_DMA_DIRECTION_PERIPH_TO_MEMORY;
xfer_cfg_tim2_cc4_dma.src_inc = HAL_DMA_SRC_ADDR_FIXED;
xfer_cfg_tim2_cc4_dma.dest_inc = HAL_DMA_DEST_ADDR_INCREMENTED;
xfer_cfg_tim2_cc4_dma.src_data_width = HAL_DMA_SRC_DATA_WIDTH_WORD;
xfer_cfg_tim2_cc4_dma.dest_data_width = HAL_DMA_DEST_DATA_WIDTH_WORD;
xfer_cfg_tim2_cc4_dma.priority = HAL_DMA_PRIORITY_LOW_WEIGHT_HIGH;
if (HAL_DMA_SetConfigPeriphLinkedListCircularXfer(&hLPDMA1_CH2, &DMA_Node_TIM2_CC4, &xfer_cfg_tim2_cc4_dma) != HAL_OK)
{
return NULL;
}
/* Enable the interruption for LPDMA1_CH2 */
HAL_CORTEX_NVIC_SetPriority(LPDMA1_CH2_IRQn, HAL_CORTEX_NVIC_PREEMP_PRIORITY_5, HAL_CORTEX_NVIC_SUB_PRIORITY_0);
HAL_CORTEX_NVIC_EnableIRQ(LPDMA1_CH2_IRQn);
/* Link Capture/Compare 4 DMA request handle to the TIM handle */
if (HAL_TIM_SetDMA(&hTIM2, HAL_TIM_DMA_ID_CC4, &hLPDMA1_CH2) != HAL_OK)
{
return NULL;
}
return &hTIM2;
}
void mx_tim2_deinit(void)
{
(void)HAL_TIM_DeInit(&hTIM2);
HAL_RCC_TIM2_DisableClock();
HAL_RCC_TIM2_Reset();
/* De-initialize all GPIOC pins associated with TIM2 */
HAL_GPIO_DeInit(PC4_PORT, PC4_PIN);
/* Disable Timer global interrupt */
HAL_CORTEX_NVIC_DisableIRQ(TIM2_IRQn);
/* De-initialize the DMA channel */
HAL_DMA_DeInit(&hLPDMA1_CH2);
/* Disable the interruption for DMA */
HAL_CORTEX_NVIC_DisableIRQ(LPDMA1_CH2_IRQn);
}
hal_tim_handle_t *mx_tim2_gethandle(void)
{
return &hTIM2;
}
/******************************************************************************/
/* TIM2 global interrupt is managed directly in user code. */
/******************************************************************************/
/* void TIM2_IRQHandler(void)
{
}
*/
/******************************************************************************/
/* LPDMA1 channel1 global interrupt */
/******************************************************************************/
void LPDMA1_CH2_IRQHandler(void)
{
HAL_DMA_IRQHandler(&hLPDMA1_CH2);
}I attached the ioc2 file.
Regards,
Gil