Skip to main content
DLech.2
Associate
September 25, 2026
Question

Incomplete project generation from example

I tried to create a project based on an existing STM32CubeC5 example and build it from command line.

I am working on Linux and had the same issue on Ubuntu and Fedora.

I opened CubeMX2 (Version: 1.1.1) and selected the “freertos_low_power.ioc2” under “STM32CubeC5/examples/middleware/freertos/low_power/NUCLEO-C562RE”, saved it to my new project folder as recommend via “save as” and tried to generate the CMake project.

Direct at generation start I got the error message shown below, but a “good looking” project folder was still generated.

Project extraction failed:
=========================================================
Example Path: /home/lecd/devel/STM32CubeC5/examples/middleware/freertos/low_power/NUCLEO-C562RE/freertos_low_power.ioc2
Project Name: low_power
Board Name: NUCLEO-C562RE
Format: CMake
Project Directory: /home/lecd/devel/stm32c5_demo
SW Pack Root: /home/lecd/devel/STM32CubeC5
Extract STM32CubeMX2 project with the selected format: false
Copy Only Dependencies: true
Exact Match Project Name: true
=========================================================
[ERROR] No CMake project for this example, please select another format. Available formats for this example are: ["ewarm", "open-cmsis", "cmake"]
{"status":"error","messages":{"errors":["No CMake project for this example, please select another format. Available formats for this example are: [\"ewarm\", \"open-cmsis\", \"cmake\"]"],"warnings":[],"infos":[]}}

The following CMake config looked fine:

[0]lecd@lecd:~/devel/stm32c5_demo/freertos_lowpower_test_cmake/build$ cmake -G Ninja -DCMAKE_BUILD_TYPE=debug_GCC_NUCLEO-C562RE -DTOOLCHAIN_FILE=GCC.14.3.1.cmake ..
-- The C compiler identification is GNU 14.2.1
-- The CXX compiler identification is GNU 14.2.1
-- Configuring done (1.4s)
-- Generating done (0.1s)
-- Build files have been written to: /home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/build

When I tried to run “ninja” I got the following error:

/home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/main.c: In function 'background_task_entry':
/home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/main.c:140:30: error: 'NOTIFICATION_VALUE_UNKNOWN' undeclared (first use in this function)
140 | uint32_t ulNotifiedValue = NOTIFICATION_VALUE_UNKNOWN;
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
/home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/main.c:140:30: note: each undeclared identifier is reported only once for each function it appears in
/home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/main.c:155:14: error: 'NOTIFICATION_VALUE_SUCCESS' undeclared (first use in this function)
155 | case NOTIFICATION_VALUE_SUCCESS:
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
/home/lecd/devel/stm32c5_demo/freertos_lowpower_test_cmake/main.c:160:14: error: 'NOTIFICATION_VALUE_ERROR' undeclared (first use in this function)
160 | case NOTIFICATION_VALUE_ERROR:
| ^~~~~~~~~~~~~~~~~~~~~~~~
[35/45] Building C object CMakeFiles/freertos_lowpower_test.dir/stm32c5xx_drivers/hal/stm32c5xx_hal_flash_itf.c.obj
ninja: build stopped: subcommand failed.

Comparing the generated folder with the example it turned out that the “mx_freertos_app.{c,h}” files are simply missing the actual example application code.

After porting the application code over the build worked just fine.

 

Questions:

  • Is the first error during generation a real problem and if so, when will it get fixed?
  • Is the missing app code a result of the initial generation error, a separate issue or designed behavior?
  • When (if ever) will it be possible to transfer board or MCU config to a different compatible board or MCU in CubeMX2? 

 

1 reply

ST Technical Moderator
October 5, 2026

Hello ​@DLech.2 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: CDM0066237 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om