Skip to main content
ebrombaugh1
Associate III
Apr 15, 2026 5:44 AM UTC
Solved

CubeMX2: I2S Sample rate calculation does not match value computed in hardware by HAL

In CubeMX2 when configuring the I2S peripheral on an STM32C542 running from a clock of 144MHz and selecting an audio clock rate of 96000Hz, CubeMX2 computes a nearest reachable frequency of 97826Hz (I2SDIV = 23, ODD = 0). When code is generated and run on actual hardware, the HAL2 I2S driver computes a different value of 95744Hz (I2SDIV = 23, ODD = 1). The HAL2 hardware value has less error from the desired 96000Hz than the value reported by CubeMX2, but the CubeMX2 value may be used in designing other aspects of the firmware and result in unexpected performance.

 

ebrombaugh1_0-1776231757798.png

 

Saket_OmBest answer
ST Technical Moderator
Jun 25, 2026 2:22 PM UTC

Hello ​@ebrombaugh1 

The issue has been solved in the new STM32C5 Ecosystem release 2.1.0. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

2 replies

ST Employee
Apr 15, 2026 9:20 AM UTC

Hello @ebrombaugh1,

I have escalated the issue to the relevant team for resolution. It is being tracked internally under ticket number CDM0061754.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
Saket_OmBest answer
ST Technical Moderator
Jun 25, 2026 2:22 PM UTC

Hello ​@ebrombaugh1 

The issue has been solved in the new STM32C5 Ecosystem release 2.1.0. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om