I understand that you’re unable to install STM32CubeMX2 v1.1.2 on Linux Mint 22.3 XFCE. Could you please share the exact error message and explain how you launched the installer? If possible, please also attach a screenshot and any output from the installation attempt.
Any details you can provide will help us reproduce the issue and investigate it.
Best regards, Oussama
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Linux Mint is running in Oracle VM VirtualBox, this poses no issue for CubeMX or CubeProgrammer, and I trust it will be the same for CubeMX2. RAM is set to 8GB. Number of CPUs: 6. Video memory: 128MB (the maximum).
The host operating system is also Linux Mint
I perform the installation by running `sudo ./stm32cubemx 2-1.1.2-X64-Linux-installer` from the folder where the installation file is located. After doing this, a grey, empty rectangle appears, with the text "STM32CubeMX2 installer 1.1.2" displayed at the top.
Does anyone have experience installing CubeMX2 on a Linux distribution where the program actually works? If so, could you let me know which distribution it is? I’d like to give that one a try.
Installation on VM Installation with 3D acceleration enabled does not work. Installation without 3D acceleration enabled works fine. However, the program itself does not work. Installed on the Linux host system (also Linux Mint) as user; the program works perfectly, as far as I can tell for now. That works for me, too.