Skip to main content
Associate II
May 6, 2026 4:07 PM UTC
Solved

404 Errors Installing CubeMX2 Packs

Hello,

I am using CubeMX2 Version 1.0.0 on macOS Silicon.

Various software packs fail to install with a 404 error like this:

Could not fetch content of pack-URL: https://developer.st.com/st-pack-server/api/v1/pack/STMicroelectronics.rot_provisioning.2.0.0.pack, got: 404 - Not Found

The following packs where tested and failed:

Is this an error on my side, similar to the proxy or certification issues I saw in other tickets or are these packs just not available YET?

Secondly, I see support packs for e.g. the L4 MCU series: "stm32l4xx_dfp". What is the point of having these packs if CubeMX2 will not support these MCUs?

Oussama_TROUDI
Oussama_TROUDIBest answer
ST Technical Moderator
Jun 25, 2026 2:55 PM UTC

Hello ​@User_MV 

 

Following the release of STM32C5 Release 2.1.0, the following packs:  rot_provisioning, eeprom_emulation, mcuboot, fileX and usbX are now available and can be installed via Pack Manager in STM32CubeMX2.

 

Regards,
Oussama

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

User_MVAuthor
Associate II
May 8, 2026 3:22 PM UTC

Problem persists with version 1.0.1.

Tested with mcuboot pack.

Oussama_TROUDI
ST Technical Moderator
May 8, 2026 4:14 PM UTC

Hello @User_MV 

Regarding the first point, I have submitted an internal ticket for further analysis. We will keep you posted. 

In the meantime, please download the required packs from STM32 Package Creator 'https://dev.st.com/stm32pc/' as you did before, and install them locally in STM32CubeMX2. 

Internal ticket number: CDM0062505 (This is an internal tracking number and is not accessible or usable by customers).


Regarding the Second point: It was decided to display all packs available on the server and only indicate their compatibility with STM32CubeMX2:

  • Yes: ST pack compatible with this MX2 version
  • No: ST pack not compatible with this MX2 version
  • Unknown: ST pack without compatibility info, or not an ST pack

Note: Any displayed pack can still be installed, even if it is not compatible.

Oussama_TROUDI_0-1778254407245.png

Regards,
Oussama

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Oussama_TROUDI
Oussama_TROUDIBest answer
ST Technical Moderator
Jun 25, 2026 2:55 PM UTC

Hello ​@User_MV 

 

Following the release of STM32C5 Release 2.1.0, the following packs:  rot_provisioning, eeprom_emulation, mcuboot, fileX and usbX are now available and can be installed via Pack Manager in STM32CubeMX2.

 

Regards,
Oussama

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.