Skip to main content
Katzenberger.Michael
Associate III
Oct 17, 2016 7:38 PM UTC
Question

wrong return value for osSignalWait ?

Posted on October 17, 2016 at 21:38 Hi ! I'm using freeRTOS with STM32CubeMX. While playing with signals for inter-thread communication I came across the different return value of function osSignalSet() The CMSIS standard states:

int32_t osSignalSet(osThreadId thread_id, int32_t signals)
Parameters
[in] thread_id thread ID obtained by osThreadCreate or osThreadGetId.
[in] signals specifies the signal flags of the thread that should be set.
Returns
previous signal flags of the specified thread or 0x80000000 in case of incorrect parameters.

But STM32CubeMX creates:

/**
* @brief Set the specified Signal Flags of an active thread.
* @param thread_id thread ID obtained by \ref osThreadCreate or \ref osThreadGetId.
* @param signals specifies the signal flags of the thread that should be set.
* @retval osOK if successful, osErrorOS if failed .
* @note MUST REMAIN UNCHANGED: \b osSignalSet shall be consistent in every CMSIS-RTOS.
*/
int32_t osSignalSet (osThreadId thread_id, int32_t 

signal

)
And indeed the only return values are osErrorOS (=255) or osOK (=0) ! Same applies to function osSignalClear() Bug or feature ??? ;) Best regards, Michael. #stm32cubemx #stm32cube-free-rtos-cmsis
This topic has been closed for replies.

3 replies

ST Technical Moderator
Oct 31, 2016 9:34 AM UTC
Posted on October 31, 2016 at 10:34

Dear User,

Thank you for highlighting this issue.

Please note that your feedback is reported internally and it is under review.

Best Regards

STM32.forum

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jeanne Joly
Associate
Jan 9, 2017 3:34 PM UTC
Posted on January 09, 2017 at 16:34

Hi

Katzenberger.Michael

,

Your bug has been solved and will be delivered in CubeMX4.

BR.

Eric Dampierre

Jeanne Joly
Associate
Jan 10, 2017 11:46 AM UTC
Posted on January 10, 2017 at 11:46

Hi again

Katzenberger.Michael

,

For your information, I have a recent update from our development team and the bug will be delivered in CubeMX4.21 (instead ofCubeMX4.20).

BR. Eric Dampierre