Skip to main content
pohtv
Associate
May 26, 2017
Question

Why STM32CubeMX No More Generating sysmem.c?

Posted on May 26, 2017 at 13:35

Hi,

How do I enable the STM32CubeMX version 4.21.0 to generate sysmem.c file under startup folder? The file seems to be missing. The older version of STM32CubeMX automatically generates it.

#stm32
    This topic has been closed for replies.

    7 replies

    ST Technical Moderator
    May 30, 2017
    Posted on May 30, 2017 at 12:23

    Hi, 

    I will forward your feedback internally to our CubeMx team to inform you about the taken explanation.

    Thanks

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Jeanne Joly
    Associate
    January 22, 2018
    Posted on January 22, 2018 at 16:35

    Hi

    Poh.Tze_Ven

    ,

    Sorry for the late answer.

    Before, we were pointing directly on the system.c file under FW package and now, at the first generation, it is copied from the FW src folder to CubeMX src folder.

    Hope it will help you.

    BR

    Associate II
    March 19, 2024

    After I updated CubeMX 6.9 to 6.11.0 and migrated my project to new version I have a problem that everytime I re-generate the code the compiler complains missing syscalls.c, sysmem.c files. This files doesn't exist anywhere in the project neither CubeMX folder. The code generator always places this files in generated Makefile at the end of C_SOURCES list and I have to manually delete this 2 lines. Is there some option to not place this non-existing files in Makefile?

    David Littell
    Senior II
    March 19, 2024

    Don't hijack threads - create your own.

    LLeva.1
    Associate II
    April 5, 2024

    ?

    Visitor II
    May 27, 2025

    Hi,

    I had same problem with Version 6.14.1 using stm32h757.

    Following solves it:

    Goto "Pinout & Configuration" -> "Trace and Debug": Switch on "DEBUG".
    After that the sysmem.c is generated in CM7 and CM4.

    The answer is late, but problem still there and maybe new people may found that helpful.

    Regards,
    Clemens