Skip to main content
tinu
Associate
Feb 8, 2019 5:48 AM UTC
Question

Why simpel MX project will not compile: arm_math.h is missing

Using MX 5.0.1 and create a new project "PrjA" for STboard STNM32F401 Nucleo. No changes or configs. Then generate code and open in TrueStudio. Compilation fails because of:

..\Drivers\CMSIS\DSP_Lib\Source\FilteringFunctions\arm_fir_decimate_init_q15.c:41:22: fatal error: arm_math.h: No such file or directory

But the arm_math.h is existing in the folder C:\STM32\PrjA\Drivers\CMSIS\Include.

Is that normal that I have to add a library path to a MX generated project to compile without error?

Then I try to add this path to the project / properties / Includes or Library Paths and get even worse compilation error missing include files.

This topic has been closed for replies.

1 reply

tinu
tinuAuthor
Associate
Feb 8, 2019 6:23 AM UTC

Up's choosing the correct Toolchain/IDE "TrueSTUDIO" help's a lot. Compilation is now OK.