Skip to main content
JoniS
Senior
December 29, 2018
Question

Why is MX_xxxx_Init()(HAL drivers) getting stuck in infinity loop if LL_RCC driver is used, instead of its HAL counterpart?

  • December 29, 2018
  • 3 replies
  • 632 views

Mcu: STM32F446RET6

STM32CubeMX 5.0.0 (STM32Cube V1.0)

So, yeah i figured out that if i use LL_RCC_DRIVER and then any periephal which only does have HAL_driver implemented by ST, it will get stuck in infinity loop in the corresponding init function.

ie.

 if (HAL_CAN_Init(&hcan1) != HAL_OK) // <<- permanently stuck
 {
 Error_Handler();
 }

and the actual infinity loop is below.

 while ((hcan->Instance->MSR & CAN_MSR_SLAK) != RESET) // <-- Always true
 {
 if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE) // <-- never true
 {
 /* Update error code */
 hcan->ErrorCode |= HAL_CAN_ERROR_TIMEOUT;
 
 /* Change CAN state */
 hcan->State = HAL_CAN_STATE_ERROR;
 
 return HAL_ERROR;
 }
 }

Now i ask, why i'm able to select LL and HAL driver mixture from cubeMX if it does not work anyway, using HAL_RCC driver and this proplem is gone, but that is not a fix.

Second, MX_CAN2_Init() always results into HAL_ERROR?

This topic has been closed for replies.

3 replies

S.Ma
Principal
December 29, 2018

Some other fresh thread talk about Systick not working well with latest CubeMX.

Maybe there is a link here?

HAL_GetTick() relies on Systick.

If this one is not working, yes, the timeout may not happen as time is "frozen"?

JoniS
JoniSAuthor
Senior
December 29, 2018

I'm pretty sure it did return 0 always(need to check later again to be sure), which would make the timeout not work.​ But that is only if I try to use low level driver for the RCC, using HAL driver for RCC and it does work.(HAL_GetTick() does return values)

​

Well or atleast the init works, can't get the can loopback work properly, but that is issue for another topic.​

Tesla DeLorean
Guru
December 29, 2018

The SysTick_Handler needs to minimally call HAL_IncTick() for the counter to advance. The SystTick also needs to have sufficient preempt priority to cut through other callbacks or interrupts that have dependency.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..