Associate II
December 5, 2025
Question
Why in CubeMX the sum of the two parameters must be be 32?
- 1 reply
- 537 views
New question split from this thread.
Hello,
Thank you for your response. I have double-checked and found that the 6.10 version also cannot be configured in this way. I will adopt the single-line mode on the next hardware version.
However, there is still a question regarding the configuration of can in version 6.16. Why must the sum of the two parameters in the following figure be 32? Otherwise, there will be a warning. In version 6.13, this issue does not exist.

The attachment contains the relevant IOC files.