Skip to main content
caleb
Associate III
Jun 11, 2019 3:31 PM UTC
Question

Why can't I enable all 4 SAI ports on STM32H750/STM32H743?

Hello,

I am attempting to use all 4 sai ports as one large synchronous audio device.

The I want SAI1A to be the master, and SAI1B, SAI2A, SAI2B, SAI3A, SAI3B, SAI4A, SAI4B to all be synchronous slaves to the SAI1A.

I am able to configure them all, except for SAI4B, which says it's in conflict with SAI1B synchronous slave. I'm using the internal synchronous signals, all synchronous slaves are marked as, "Synchronous with other SAI, SAI1". But just 4B says it's in conflict.

I assume if I configure it manually, it'll probably work fine...

Thanks

-Caleb

This topic has been closed for replies.

4 replies

Amel NASRI
ST Technical Moderator
Jun 28, 2019 9:54 AM UTC

Hi @caleb​ ,

This issue seems to be similar to the one reported in this question.

I add @Khouloud ZEMMELI​  to let us know if there is any update on this regard.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Khouloud ZEMMELI
ST Employee
Jul 1, 2019 7:18 AM UTC

​Hello , For : this question : According to our development team, the product supports only 6 microphones.

Request invalid.

Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee
Jul 1, 2019 8:53 AM UTC

​@caleb​  , could you please share more info about your request? which version of CubeMX?

Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee
Jul 3, 2019 8:12 AM UTC

hi ​@caleb​ , Tested with H743IIKx and it works fine , for H750 it will be fixed .

Best Regards,

Khouloud.