STM32CubeIDE is integrating part of STM32CubeMX product. Being short I would say integrate all STM32CubeMX features except the one dedicated to IDEs which are not STM32CubeIDE.
STM32CubeMX is IDE vendor agnostic. If STM32CubeMX you can ask to generate material for Keil, IAR, ... solutions.
If relying on integrated solution obviously only supported IDE is STM32CubeIDE itself.
If aiming to target only STM32CubeIDE maybe good idea on rely on as a whole. Integration especially if beginner may help. Up to you. In any case both working models are fully supported like using STM32CubeIDE only or STM32CubeMX and STM32CubeIDE.
STM32CubeIDE is all in one solution including devices / examples selection, device configuration, code editing, debug on target. STM32CubeMX is supporting devices / examples selection, device configuration.