Skip to main content
CChur
Associate
October 23, 2018
Question

Where can I get an actual version of the SRM32CubeF0 Firmware Package V1.5.0?

I am working on a project that integrates the cubemx-classb library, which depends on V1.5.0, and also want to use STM32CubeMX for other configuration. However, it appears that the STM32CubeF0 Firmware Package V1.5.0 configured by the STM32CubeMX tool provides outdated (v1.3.1) HAL header files. Generated initialization files are not compatible, specifically WWDG references non-existent MACROS that don't appear until V1.5.0.

This topic has been closed for replies.

4 replies

ST Technical Moderator
October 24, 2018

Hello @CChur​ ,

The STM32CubeF0 firmware package V1.5.0 is not compatible with the last version of STM32CubeMx.

According the release note of STM32CubeMx, the STM32CubeF0 firmware package V1.5.0 is used within the STM32CubeMX V4.15.0.

However, it's highly recomended to use the last available Cube firmware package and STM32CubeMX versions, since they always provide enhancement and bug fixes.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
CChur
CChurAuthor
Associate
October 24, 2018

Is it possible to get a copy of STM32CubeMX V4.15.0? For Linux?

CChur
CChurAuthor
Associate
October 24, 2018

Ok thanks. However, the STM32CubeMX tool does allow you to select previous versions of the SDK (from 'Help->Manage Embedded Packages'), and they are incorrect. For instance, configuring v1.5.0 gets you v1.3.1, v1.6.0 gets you v1.4.0, and v1.7.0 gets you v1.5.0.

Tesla DeLorean
Guru
October 24, 2018
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..