Skip to main content
KiptonM
Senior III
Jun 7, 2022 3:59 PM UTC
Question

When I setup the RANK for the ADC I want to read TemperatureSensor, VRef, IN0, IN1. But the order appears IN1, TemperatureSensor, Vref, IN0

In the MX program I set up the rank. to scan 4 values.

TemperatureSensor, VRefint, IN0, IN1.

I Initially saw this in DMA mode, But see it also happens in Discontinuous Mode.

0693W00000NrLM9QAN.pngBut when read the order is off by 1 position.

It looks like it is reading IN1, TemperatureSensor, VRefint, IN0,

Here is the relevant code.

/* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART1_UART_Init();
 MX_USART2_UART_Init();
 MX_I2C1_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 MX_ADC1_Init();
 
 /* Initialize interrupts */
 MX_NVIC_Init();
 /* USER CODE BEGIN 2 */
 
 //ADC_init();
 
 if (HAL_ADCEx_Calibration_Start(&hadc1) != HAL_OK)
 {
	 print_debug_str("Did not calibrate right!");
 }
 
 //ADC_DMA_Setup();
 
 HAL_Delay(100); // Make sure print is done.
 
 {
	 char buf[100];
	 uint16_t i;
	 uint16_t refv;
	 uint16_t temp;
	 uint16_t adc_data[4];
	 for (i=0;i<50;i++)
	 {
 
		 adc_data[0] = 0xFFFF;
		 adc_data[0] = 0xFFFF;
		 adc_data[0] = 0xFFFF;
		 adc_data[0] = 0xFFFF;
		 ADC1->IER = 0; // make sure this is clear
 
		 // This should be Temperature
		 ADC1->ISR |= 2; // Clear EOC Flag
		 HAL_ADC_Start(&hadc1);
		 while ((ADC1->ISR & 2) == 0);
		 adc_data[0] = ADC1->DR;
		 ADC1->ISR |= 2;
 
		 // This should be vref
		 HAL_ADC_Start(&hadc1);
		 while ((ADC1->ISR & 2) == 0) ;
		 adc_data[1] = ADC1->DR;
		 ADC1->ISR |= 2;
 
		 // This should be a voltage -- Not connected expect 0
		 HAL_ADC_Start(&hadc1);
		 while ((ADC1->ISR & 2) == 0) ;
		 adc_data[2] = ADC1->DR;
		 ADC1->ISR |= 2;
 
		 // This should be a current -- Not connected expect 0
		 HAL_ADC_Start(&hadc1);
		 while ((ADC1->ISR & 2) == 0) ;
		 adc_data[3] = ADC1->DR;
		 ADC1->ISR |= 2;
 
		 refv = __HAL_ADC_CALC_VREFANALOG_VOLTAGE(adc_data[2],ADC_RESOLUTION_12B);
		 temp = __HAL_ADC_CALC_TEMPERATURE(refv,adc_data[1],ADC_RESOLUTION_12B);
 
 
		 sprintf(buf,"%4u ADC Discontinuous readings: %04X %04X %04X %04X TempC: %u, Vref mV: %u\r\n",i, adc_data[0],adc_data[1],adc_data[2],adc_data[3], temp, refv);
		 print_debug_str(buf);
 
		 HAL_Delay(100); // make sure print has time to finish.
	 } // for
 }
 
 while(1); // Stop here while debugging ADC

Looking at the printout it is:

 0 ADC Discontinuous readings: 0020 039D 05D7 0001 TempC: 27, Vref mV: 3331
 1 ADC Discontinuous readings: 0001 039F 05D6 0002 TempC: 27, Vref mV: 3333
 2 ADC Discontinuous readings: 0000 03A3 05E4 0000 TempC: 26, Vref mV: 3302
 3 ADC Discontinuous readings: 0001 03A5 05E4 0000 TempC: 26, Vref mV: 3302
 4 ADC Discontinuous readings: 0002 03A5 05E3 0001 TempC: 27, Vref mV: 3304
 5 ADC Discontinuous readings: 0001 03A5 05E2 0001 TempC: 27, Vref mV: 3306
 6 ADC Discontinuous readings: 0001 03A5 05E4 0001 TempC: 26, Vref mV: 3302
 7 ADC Discontinuous readings: 0001 03A4 05E2 0001 TempC: 27, Vref mV: 3306
 8 ADC Discontinuous readings: 0002 03A6 05E3 0000 TempC: 27, Vref mV: 3304
 9 ADC Discontinuous readings: 0002 03A5 05E2 0000 TempC: 27, Vref mV: 3306
 10 ADC Discontinuous readings: 0001 03A7 05E4 0001 TempC: 27, Vref mV: 3302
 11 ADC Discontinuous readings: 0002 03A5 05E4 0001 TempC: 26, Vref mV: 3302
 12 ADC Discontinuous readings: 0002 039F 05D8 0001 TempC: 27, Vref mV: 3328
 13 ADC Discontinuous readings: 0002 03A3 05DF 0001 TempC: 27, Vref mV: 3313
 14 ADC Discontinuous readings: 0001 03A6 05E3 0001 TempC: 27, Vref mV: 3304
 15 ADC Discontinuous readings: 0002 03A6 05E3 0000 TempC: 27, Vref mV: 3304
 16 ADC Discontinuous readings: 0001 03A5 05E4 0001 TempC: 26, Vref mV: 3302
 17 ADC Discontinuous readings: 0001 03A6 05E3 0000 TempC: 27, Vref mV: 3304
 18 ADC Discontinuous readings: 0002 03A5 05E4 0000 TempC: 26, Vref mV: 3302
 19 ADC Discontinuous readings: 0002 03A5 05E3 0000 TempC: 27, Vref mV: 3304
 20 ADC Discontinuous readings: 0001 03A5 05E3 0001 TempC: 27, Vref mV: 3304
 21 ADC Discontinuous readings: 0002 03A6 05E4 0002 TempC: 27, Vref mV: 3302
 22 ADC Discontinuous readings: 0002 03A6 05E4 0001 TempC: 27, Vref mV: 3302
 23 ADC Discontinuous readings: 0002 03A3 05DF 0000 TempC: 27, Vref mV: 3313
 24 ADC Discontinuous readings: 0001 03A5 05E4 0001 TempC: 26, Vref mV: 3302
 25 ADC Discontinuous readings: 0002 03A6 05E2 0000 TempC: 27, Vref mV: 3306
 26 ADC Discontinuous readings: 0003 03A6 05E3 0001 TempC: 27, Vref mV: 3304
 27 ADC Discontinuous readings: 0001 03A5 05E4 0001 TempC: 26, Vref mV: 3302
 28 ADC Discontinuous readings: 0002 03A7 05E3 0001 TempC: 27, Vref mV: 3304
 29 ADC Discontinuous readings: 0002 03A6 05E2 0001 TempC: 27, Vref mV: 3306
 30 ADC Discontinuous readings: 0002 03A7 05E3 0001 TempC: 27, Vref mV: 3304
 31 ADC Discontinuous readings: 0002 03A6 05DF 0000 TempC: 28, Vref mV: 3313
 32 ADC Discontinuous readings: 0002 03A5 05E2 0002 TempC: 27, Vref mV: 3306
 33 ADC Discontinuous readings: 0001 03A5 05E3 0001 TempC: 27, Vref mV: 3304
 34 ADC Discontinuous readings: 0002 03A5 05E3 0001 TempC: 27, Vref mV: 3304
 35 ADC Discontinuous readings: 0002 03A0 05DA 0000 TempC: 27, Vref mV: 3324
 36 ADC Discontinuous readings: 0001 03A6 05E4 0001 TempC: 27, Vref mV: 3302
 37 ADC Discontinuous readings: 0001 03A6 05E2 0001 TempC: 27, Vref mV: 3306
 38 ADC Discontinuous readings: 0001 03A5 05E5 0002 TempC: 26, Vref mV: 3300
 39 ADC Discontinuous readings: 0001 03A7 05E4 0001 TempC: 27, Vref mV: 3302
 40 ADC Discontinuous readings: 0002 03A6 05E2 0001 TempC: 27, Vref mV: 3306
 41 ADC Discontinuous readings: 0001 03A6 05E4 0000 TempC: 27, Vref mV: 3302
 42 ADC Discontinuous readings: 0002 03A7 05E3 0000 TempC: 27, Vref mV: 3304
 43 ADC Discontinuous readings: 0001 03A7 05E3 0001 TempC: 27, Vref mV: 3304
 44 ADC Discontinuous readings: 0001 03A6 05E3 0000 TempC: 27, Vref mV: 3304
 45 ADC Discontinuous readings: 0002 03A6 05E4 0001 TempC: 27, Vref mV: 3302
 46 ADC Discontinuous readings: 0002 03A5 05E4 0000 TempC: 26, Vref mV: 3302
 47 ADC Discontinuous readings: 0001 03A6 05E5 0000 TempC: 27, Vref mV: 3300
 48 ADC Discontinuous readings: 0001 03A1 05DB 0000 TempC: 27, Vref mV: 3322
 49 ADC Discontinuous readings: 0001 03A6 05E3 0001 TempC: 27, Vref mV: 3304

For a sanity check I converted the second one (adc_data[1]) to a temperature, and the third one )adc_data[2] to a voltage in mV, and they confirm they are in the wrong place.

The generated code looks right.

/**
 * @brief ADC1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 
 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.LowPowerAutoPowerOff = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.DiscontinuousConvMode = ENABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_39CYCLES_5;
 hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_VREFINT;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}

Why is the order wrong?

How do I fix it?

Thanks, in advance.

This topic has been closed for replies.

3 replies

KiptonM
KiptonMAuthor
Senior III
Jun 7, 2022 8:04 PM UTC

I did not change anything in the MX program. I did change the the oversample to 8 in the ADC_CFGR2 register and set OVSE to enable it.

Now the order is correct!

In this line are the values as read from the ADC_DR (x8) Temp, Vref, AN0, AN1

ADC Discontinuous 8 readings: 1D37 2F28 0007 0020 FFFF FFFF FFFF FFFF

Here I shifted right 3 positions each of the values. And converted the first to Temperature in C, Temperature in F * 10, and second The Reference Voltage in mV. They all look good and are in the right position.

ADC Discontinuous readings: 03A6 05E5 0000 0004 TempC:  27, TempF*10: 806, Vref mV: 3300

I tried to run the routine 10 times but only got values the first time. I am going to hunt that down next.

HCui
Associate II
Jun 11, 2022 12:11 AM UTC

I also ran into this bug recently. My solution is adding a delay (1ms) after stopping the DMA. It is confusing.

Javier1
Principal
Jun 13, 2022 7:34 AM UTC

Same/similar thing happened to me, i wasnt giving the DMA enough time to fill the ADC readings buffer, i fixed it by speeding up the ADC triggers

hit me up in https://www.linkedin.com/in/javiermuñoz/