What is the correct default value for RCC_HSICALIBRATION_DEFAULT for STM32L431? It is going to be corrected in the HAL libraries?
Hi,
I have an accuracy problem with the HSI16 of my STM32L431. It is really outside specifications, over 10% from 16MHz.
I have discovered that during the initialitation of the RCC, the value of RCC_HSICALIBRATION_DEFAULT is 0x40, like in the datasheet
default value, but in AN4736 it´s seems to be 0x10.
The fact is that is I change this value to 0x10, the HSI16 clock is generated correctly, but if I let the MXCube do it by itself, the value is taken from the "stm32l4xx_hal_rcc.h" where:
#if defined(RCC_ICSCR_HSITRIM_6)
#define RCC_HSICALIBRATION_DEFAULT 0x40U /*!< Default HSI calibration trimming value 64 on devices other than STM32L47x/STM32L48x */
#else
#define RCC_HSICALIBRATION_DEFAULT 0x10U /*!< Default HSI calibration trimming value 16 on STM32L47x/STM32L48x devices */
#endif /* RCC_ICSCR_HSITRIM_6 */
so it takes 0x40 default value.
Is the datasheet wrong?
Is possible to correct it using the MXCube?