Skip to main content
LFerg.2
Associate
Dec 17, 2020 9:25 PM UTC
Question

We have downloaded the STSW-IOD01 firmware for the Nucleo-L073rz board. The STSW-IOD01 project is not set up in a format able to be used with the STM32CubeMx. Is there some way to convert it so we can use it with the STM32CubeMx environment?

We have selected the Nucleo-L073rz board in STM32CubeMx, created a project and are copying the code from STSW-IOD01 into the new project but this is very tedious and prone to errors.

Also, please note that the STSW-IOD01 firmware comes preloaded in the Nucleo-073rz board.

This topic has been closed for replies.