Skip to main content
WBayo
Associate
Sep 5, 2019 3:36 PM UTC
Question

Using the IDE Version: 1.0.2 Build: 3566_20190716-0927 (UTC) 'DMA continuous request' entry stays in DISABLED condition, no way to set it to ENABLED

Circular buffer DMA is defined for an ADC.

I want it to start and continue to convert forever.

If I manually correct the init procedure which was generated, that works well

This topic has been closed for replies.

5 replies

Amel NASRI
ST Technical Moderator
Sep 24, 2019 8:34 AM UTC

which device are you using?

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
WBayo
WBayoAuthor
Associate
Sep 24, 2019 10:05 AM UTC

STM32F446

Amel NASRI
ST Technical Moderator
Sep 24, 2019 10:46 AM UTC

Hi @WBayo​ ,

This seems to be the same issue as DMA Continuous Requests - Not selectable option on STM32F446RE Nucleo Board.

@Nesrine.JLASSI​ : could you please have a look to both discussions?

Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
WBayo
WBayoAuthor
Associate
Sep 24, 2019 12:19 PM UTC

Yes, indeed.

It is just what I did to go around the bug in the IDE.

I am now using the version   STM32CubeMX 5.3.0.201907110903

and the bug is still not corrected.

Nesrine.JLASSI
Visitor II
Sep 24, 2019 3:33 PM UTC

​Hello @WBayo​ 

Thanks for the feedback, the problem is known, it will be corrected in the next STM32CubeMX release.

Best regards,

Nesrine