Skip to main content
MK..1
Associate III
November 30, 2023
Question

using fatfs iand azure rtos

Hi

When selecting azure RTOS in CubeMX, it is not possible to select FATFS. FATFS is greyed out. It is only allowed to choose FileX. Why?

Thx

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
November 30, 2023

Because it's Microsoft, properly integrated and licensed.

ST hasn't updated FATFS in something like 6 or 7 years, it has some nasty bugs, and clearly no one is interested in integration and testing tasks. Heck that would require regression testing over a dozen STM32 families.

Stop relying on code generators to create code and make choices. If you want different outcomes, make different choices..

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KDJEM.1
ST Technical Moderator
December 5, 2023

Hello @MK..1 ,

To check the issue, could you please precise:

Which STM32 devices are you using?

Which STM32CubeMx version are you using?

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
MK..1
MK..1Author
Associate III
December 5, 2023

I am using STM32F446ZCJx and STM32CubeIDE Version: 1.14.0 and

STM32Cube FW_F4 V1.27.1

KDJEM.1
ST Technical Moderator
December 6, 2023

Hi @MK..1 ,

I reported this issue internally.

Internal ticket number: 168051 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution in STCommunity :)

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.