Skip to main content
davidregan9
Associate III
Sep 17, 2019 7:33 AM UTC
Question

Using .extSettings file

In the help document concerning .extSettings file the information is unclear.

As I read it the Groups section is supposed to create/add directories and files.

It does not. I have generated the project for SystemWorkbench and EWarm.

I downloaded a test version of IAR to verify. None of the directories or files are added as described.

The only change I can find is an entry in .mxproject file.

The specified file is added to SourceFiles in PreviousUsedSW4STM32Files section.

Can anybody explain how to use the Groups section.

  •  

This topic has been closed for replies.

9 replies

davidregan9
Associate III
Sep 17, 2019 8:09 AM UTC

Hi @Markus GIRDLAND​ do you have any insight on this. Nobody seems inclined to reply

Markus GIRDLAND
ST Employee
Sep 18, 2019 10:05 AM UTC

I'm afraid I'm not much help here. I don't know a lot about MX/SW4STM32.

What documentation are you reading and where are you creating groups?

davidregan9
Associate III
Sep 18, 2019 10:26 AM UTC
Hi Markus
It was UM1718.pdf Rev 29 Page 193.
I’ve also noticed that STM3CubeIDE will not open template files
Regards
Dave Regan
davidregan9
Associate III
Sep 18, 2019 10:56 AM UTC

Hi @Nawres GHARBI​ Do you have any insight in to this problem

Khouloud ZEMMELI
ST Employee
Oct 14, 2019 10:08 AM UTC

​Hello @davidregan9​ ,

For IAR, it works fine , problem appears with SW4STM32.

This issue will be fixed in the next CubeMX release.

Best Regards,

Khouloud.

Khouloud ZEMMELI
ST Employee
Jan 7, 2020 11:03 AM UTC

the .extsettings file can not create files and directories that do not exist but allows you to add additional settings witch can be used when external tools call STM32CubeMX to generate the project and require specific project settings.

Regards,

Khouloud.

davidregan9
Associate III
Jan 7, 2020 11:33 AM UTC
HI Khouloud
Am I correct in thinking then that I could create a script to handle
the directory structure and then from this script modify .extSettings file
and launch mxCube with options from the script to generate the project?
If this is the case do you have any examples?
Regards
Dave Regan