Skip to main content
TFlac
Associate III
Aug 19, 2019 1:21 AM UTC
Question

Using a STM32F303RE Nucleus 64 eval board. Where are the Physical pins defined in a HAL / LL design flow.

Hello ST Community, I purchased the Nucleus 64 Eval board for the STM32F303RE part and downloaded all the necessary tools. I moved from CubeIDE to SW4STM32 as there are more examples available. I'm using UM1766 which outlines STM32CubeF3 flow very well. I am able to compile and load the example designs just fine. I'm now at the stage of writing my code into this Pre-Initialized project. What I can't figure out in the INITIALIZED project is where are the physical PINS defined. I am totally aware of all the files that the MX/SW4STM32 create via UM1786. Without digging super deep into the great work that the HAL flow has done, I still want to look through the PROJECT files and see where the physical pins are defined. 

In my MAIN.c, I see PC.13 as my INTERRUPT pin in COMMENTS, this is the only way I know PC.13 is the PIN. The MAIN.c refers to this PIN as "EXTI line 15_10" which is connected to PC.13. I would also like to know what suffix "15_10" means.

Which file should I look into to see these physical PIN assignments? There has to be some file that shows this LABEL connected to the physical PIN.

Thanks for the great help.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Aug 19, 2019 1:50 AM UTC

Pins are often configured in the MSP file

>> I would also like to know what suffix "15_10" means.

Means 10 thru 15 inclusive. PC13 would fall within that range

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andreas Bolsch
Lead III
Aug 19, 2019 7:28 AM UTC

Well, not sure which one you're actually looking for:

  • The file where CubeMX stores the project setting (and the pin selection in particular) is STM32CubeMX/db/plugins/boardmanager/boards/A32_Nucleo_NUCLEO-F303RE_STM32F303RE_Board.ioc.
  • The generated file containing the pin selection is STM32Cube_FW_F3_V1.10.0/Drivers/BSP/STM32F3xx-Nucleo/stm32f3xx_nucleo.h. Just skim the project's *.h and *.c files for header files and check each one in turn ...