Skip to main content
jgauthier
Senior
July 28, 2023
Solved

Using a MX25L3233F

I'm looking at using the MX25L3233F for flash storage.  This is a serial NOR device.  It appears to support QuadSPI, but it also appears to support regular SPI:

"MX25L3233F features a serial peripheral interface and software protocol allowing operation on a simple 3-wire
bus while it is in single I/O mode. The three bus signals are a clock input (SCLK), a serial data input (SI), and a
serial data output (SO). Serial access to the device is enabled by CS# input"

I'm planning on using this with an STM32G03 series, which does not support QuadSPI, but does support SPI.

Am I being too naïve to think I can use this as a regular SPI device and just use it for storage?

 

This topic has been closed for replies.
raptorhal2
raptorhal2Best answer
Lead
July 28, 2023

Its "single I/O mode" appears to be regular SPI. You can confirm this by reading the data sheet, which should have timing diagrams for all the modes supported. The device default is probably standard SPI.

.

2 replies

raptorhal2
raptorhal2Best answer
Lead
July 28, 2023

Its "single I/O mode" appears to be regular SPI. You can confirm this by reading the data sheet, which should have timing diagrams for all the modes supported. The device default is probably standard SPI.

.

jgauthier
jgauthierAuthor
Senior
July 28, 2023

The datasheet clock diagram seems to support SPI modes 0 and 3. So we'll give it a shot.