Skip to main content
Pmang.1
Associate
Apr 15, 2020 4:09 AM UTC
Question

USB CDC Device application: PC does not recognize the USB Device (Device unknow error 43)

Hello to all,

I am having problems with the CDC USB Device application. Does some one have a working USB example for STM32L1? .

 I am using latest version of CubeMx and STM32L1 firmware v1.9.0. The problem is that PC does not recognize the USB Device (Device unknow error 43).

I put together a very basic app, just to check if windows (W7 or W10) recognize the USB device but it fails.

I have been doing some HW and SW check and looks all fine but can't find the problem.

I would like to test a working USB example for STM32L1 or otherwise an older firware version just for testing.

Will be very grateful if I can get some help on this.

Thanks

This topic has been closed for replies.

2 replies

ST Technical Moderator
Apr 15, 2020 8:24 AM UTC

Hello @Pmang.1​ ,

Have a look to this FAQ: USB device not recognized, it may help you.

You can refer to the CDC example in the STM32CubeL1 firmware package and get inspired from the available one:

STM32Cube_FW_L1_V1.9.0\Projects\STM32L152D-EVAL\Applications\USB_Device\

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Apr 15, 2020 3:32 PM UTC

Try to swith the USB_DP & USB_DM pins.

USB DP & DM pins swapped would result in this.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks