Skip to main content
MStr.1
Visitor II
Jul 4, 2021 6:14 AM UTC
Question

USB CDC CubeMX generated code does not work on STM32F446RE

Hello,

I recently started using STM32 Microcontrollers, and before using STM32 Cube IDE, I used Mbed Studio for PC to USB communication using USB, and now having switched to Cube IDE, I can't seem to make the CDC class work, when I try to debug it, it shows that TxState in CDC_Transmit_FS function for some reason is never 0, and the code returns USBD_BUSY. AFAIK, I have set up the generated code correctly according to various YouTube tutorials.

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 2 */
 HAL_Delay(1000);
 uint8_t data[] = "1 2 3\n";
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
	 CDC_Transmit_FS(data,strlen(data));
	 HAL_Delay(1000);
 }
 /* USER CODE END 3 */
}
void MX_USB_DEVICE_Init(void)
{
 /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */
	USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);
	USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);
	USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);
	USBD_Start(&hUsbDeviceFS);
 
 /* USER CODE END USB_DEVICE_Init_PreTreatment */
 
 /* Init Device Library, add supported class and start the library. */
 if (USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS) != USBD_OK)
 {
 Error_Handler();
 }
 if (USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC) != USBD_OK)
 {
 Error_Handler();
 }
 if (USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS) != USBD_OK)
 {
 Error_Handler();
 }
 if (USBD_Start(&hUsbDeviceFS) != USBD_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */
 
 /* USER CODE END USB_DEVICE_Init_PostTreatment */
}
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
 uint8_t result = USBD_OK;
 /* USER CODE BEGIN 7 */
 USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
 
 if (hcdc->TxState != 0){
 return USBD_BUSY;
 }
 USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
 result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
 /* USER CODE END 7 */
 return result;
}

This topic has been closed for replies.

1 reply

Walid ZRELLI
Visitor II
Jul 13, 2021 2:37 PM UTC

Hello @MStr.1​ ,

Welcome to ST Community :smiling_face_with_smiling_eyes:

I recommend you to take a look at the examples provided in our F4 firmware package.

You can refer to the following example provided under this path : Firmware\Projects\STM32446E_EVAL\Applications\USB_Device\CDC_Standalone

I hope this helps.

BeST Regards,

Walid