Skip to main content
infor
Associate III
Dec 14, 2016 11:11 AM UTC
Solved

Upgrade of lwIP embedded in STM32CubeMX

Posted on December 14, 2016 at 12:11

Hello ST,

I'd like to ask if there are plans to upgrade the lwIP embedded (1.5) in the Cube to the recent release 2.0.0

Meanwhile, I can assure that upgrading an existing Cube project is possible!

If someone is interested, I can attempt to remember how I did :D or better, share my whole lwIP directory.

This is cool, but when the Cube regenerates the code... bye-bye 2.0.

Cheers

Giuseppe

#stm32cubemx* #lwip
This topic has been closed for replies.
Bino
BinoBest answer
ST Employee
Dec 19, 2016 9:31 AM UTC
Posted on December 19, 2016 at 10:31

Hello Giuseppe,

There is a plan to upgrade LwIP from 1.5 to 2.0.0, this will come beginning of January for STM32F7 devices in 4.19 CubeMx release and then for STM32F4 and other series in releases (4.20 and later) coming after January.

Meanwhile, your solution to put LwIP stack files (from 2.0.0 release) in your project does effectively not support a new CubeMx code generation, since CubeMx purpose is to  guarantee your are using the proper LwIP version compatible with the code generator engine in CubeMX version used.

Regards.

/Eric A.

5 replies

Bino
BinoBest answer
ST Employee
Dec 19, 2016 9:31 AM UTC
Posted on December 19, 2016 at 10:31

Hello Giuseppe,

There is a plan to upgrade LwIP from 1.5 to 2.0.0, this will come beginning of January for STM32F7 devices in 4.19 CubeMx release and then for STM32F4 and other series in releases (4.20 and later) coming after January.

Meanwhile, your solution to put LwIP stack files (from 2.0.0 release) in your project does effectively not support a new CubeMx code generation, since CubeMx purpose is to  guarantee your are using the proper LwIP version compatible with the code generator engine in CubeMX version used.

Regards.

/Eric A.

infor
inforAuthor
Associate III
Dec 20, 2016 4:47 PM UTC
Posted on December 20, 2016 at 16:47

Thank you Eric, this is good to know.

Meanwhile I can continue the development with the 'tricked' version of 2.0.0. Should I need to regenerate code with CubeMX, GIT will help me in reverting any undesired changes to lwIP.

KR

Giuseppe

ildar valetov
Associate
Aug 14, 2017 10:16 AM UTC
Posted on August 14, 2017 at 12:16

Hello! Please describe the process of upgrading LWIP to 2.0.2 version

Amel NASRI
ST Technical Moderator
Aug 14, 2017 12:59 PM UTC
Posted on August 14, 2017 at 12:59

Hi

ildar.valetov

‌,

Please a new thread for this request.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.