Skip to main content
Associate
February 24, 2025
Question

Unknown confilct in CubeMX for RTC calibration output on STM32H7R7

If I activate the calibration output 1 of the RTC, CubeMx lags and afterwards marks the options red with "unkown conflict". GPIO does not get assigned or gets cleared if done manually before. Same behavior for 1Hz and 512Hz output. OUT2 works.

 

restarted application and PC, still the same

uC: STM32H7R7L8H6H

CubeMX V6.13.0

FW versions see below

 

sh3_0-1740386549667.png

sh3_1-1740386948279.png

Thanks and regards

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
February 24, 2025

Hello @sh3 

Thank you for your contribution!

Issue has been raised to the relevant team, and it is tracked by internal ticket 203831.

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.