Skip to main content
Iman Hosseinzadeh
Associate III
Dec 27, 2020 6:15 AM UTC
Question

UART does not work properly after changing HSI to MSI in STM32L152

I am using STM32L152R8T6-A MCU. I use 3 UARTs in my project. UART buadrates are 9600 and 115200 bps.

Initially I set the clock source to HSI (16MHz) and everything worked fine. But then I decided to change the clock source to MSI (2.097 or 4.194 MHz). The program runs properly but it seems that UARTs miss some bytes, i.e. instead of getting 11 bytes, it gets the last 8 bytes.

I used the STM32CubeMX configurations and didn't change anything in initializations:

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
 PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}

Has anyone any ideas?

This topic has been closed for replies.

7 replies

KnarfB
Super User
Dec 27, 2020 7:51 AM UTC

Check with paper&pencil and/or a scope that the Cube generated baud rate generator values are accurate. Try oversamping ratio 8. Is it really missing the first bytes and correctly receiving the other ones? If so, your receive function might be called to late at slower MCU clocks.

Tesla DeLorean
Guru
Dec 27, 2020 9:30 AM UTC

Check the HAL isn't masking errors or you​ are ignoring them. Check baud rate achieved vs expect. If interrupt/callback too time consuming consider buffering and deferring work. Consider using DMA.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Iman Hosseinzadeh
Associate III
Dec 27, 2020 9:34 AM UTC

I think the clock frequency is the problem. Since HSI with 4MHz clock does not work either.

Tesla DeLorean
Guru
Dec 27, 2020 9:47 AM UTC

Or you are spending too much time processing the data. Avoid doing things in a way that takes more than one byte time to complete under interrupt context. ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Iman Hosseinzadeh
Associate III
Dec 27, 2020 2:34 PM UTC

I didn't use any interrupt. I receive the data using simple polling methid, i.e. : HAL_UART_Receive(), so no processing is done during the data receive.

TDK
Dec 27, 2020 3:41 PM UTC

> instead of getting 11 bytes, it gets the last 8 bytes.

> I receive the data using simple polling methid

It sounds like you're just not ready to receive data at the time it's being sent. Ensure whatever is sending the data waits for the MCU to be ready to receive. Use a logic analyzer to monitor pins to ensure this happens correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
shivashekar
Associate II
Dec 30, 2020 10:35 AM UTC