Skip to main content
VTOL_Aviations
Associate III
Apr 26, 2019 6:57 AM UTC
Question

UART DMA Transmit and receive not working

I'm using Atollic True Studio V 9.0 , CubeMx v5.1.0, STM32F407VG-DISC1 board and enabled DMA for UART2.

My code:

int main(void)
{
 
int i = 0;
 
 HAL_Init();
for(i = 0; i<10; i++)
 	rx_arr[i] = 0;
for(i = 0; i<10; i++)
	tx_arr[i] = i*2;
 
 SystemClock_Config();
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART6_UART_Init();
 MX_USART2_UART_Init();
 
 while (1)
 {
 
	 if( HAL_UART_Transmit_DMA(&huart2, (uint8_t*)tx_arr, 10)!= HAL_OK )
	 {
	 	 Error_Handler();
	 }
 while(UartReady != SET)
 {
 
	 }
	 UartReady = RESET;
 if( HAL_UART_Receive_DMA(&huart2, (uint8_t*)rx_arr, 10)!= HAL_OK )
	 {
	 Error_Handler();
	 }
 while(UartReady != SET)
	 {
 
	 }
	 UartReady = RESET;
 
 
}
 
}
 
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
	UartReady = SET;
}
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	UartReady = SET;
}

What I'm trying to do is fairly simple. Transmit through DMA and wait till it gets transmitted. And then receive and wait till it is received.

When I comment out the receive part(including the call back), it is going into the transmit complete call back function. But when I un-comment the receive portion, it is not going into the tx cplt call back and it is directly going into the receive cplt callback. And when I check the receive buffer I'm not getting what I expected(obviously). What could have gone wrong?

My clock settings:

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage 
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 336;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

Even though the external clock frequency is 8MHz(selected that in cubeMX too), it is showing

#if !defined (HSE_VALUE) 
 #define HSE_VALUE ((uint32_t)25000000) /*!< Default value of the External oscillator in Hz */
#endif /* HSE_VALUE */

in system_stm32f4xx.c

This topic has been closed for replies.

7 replies

Bob S
Super User
Apr 26, 2019 3:11 PM UTC

Where is your declaration for UartReady? Is it declared as "volatile"?

VTOL_Aviations
Associate III
Apr 27, 2019 4:56 AM UTC

Yes. I've declared __IO ITStatus UartReady = RESET;

Sorry for not mentioning it.

Bob S
Super User
Apr 29, 2019 4:10 PM UTC

OK. And just to be thorough, how are tx_arr and rx_arr declared? Specifically, as arrays of at least 10 elements?

What do you have connected to the other end of the serial port? Is it some program that waits to receive 10 bytes and then sends 10 bytes back? Or do you have the Tx line shorted to the Rx line for loop-back?

S.Ma
Principal
Apr 27, 2019 8:27 AM UTC

...

alouni bargougui
Associate
May 1, 2019 4:28 PM UTC

i've the same problme but i used the Keil uvision 5 with Cube Mx

please give me the terminal can be used to verified the communication carte- PC via USART

thanks a lot