Skip to main content
cb.7
Associate III
July 16, 2025
Solved

Two bugs in CubeMX 6.15 code generation with STM32U031e Low Layer libraries

The first case concerns the DAC, by setting "Output Buffer" = Disable in CubeMX, it is enabled in code generation instead, i had to add "DAC1->MCR = 0x03" in the initializations.

Cattura.PNG

 
/**
 * @brief DAC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DAC1_Init(void)
{

 /* USER CODE BEGIN DAC1_Init 0 */

 /* USER CODE END DAC1_Init 0 */

 LL_DAC_InitTypeDef DAC_InitStruct = {0};

 /* Peripheral clock enable */
 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1);

 /* USER CODE BEGIN DAC1_Init 1 */

 /* USER CODE END DAC1_Init 1 */

 /** DAC channel OUT1 config
 */
 DAC_InitStruct.TriggerSource = LL_DAC_TRIG_SOFTWARE;
 DAC_InitStruct.WaveAutoGeneration = LL_DAC_WAVE_AUTO_GENERATION_NONE;
 DAC_InitStruct.OutputConnection = LL_DAC_OUTPUT_CONNECT_INTERNAL;
 DAC_InitStruct.OutputMode = LL_DAC_OUTPUT_MODE_NORMAL;
 LL_DAC_Init(DAC1, LL_DAC_CHANNEL_1, &DAC_InitStruct);
 LL_DAC_DisableTrigger(DAC1, LL_DAC_CHANNEL_1);
 /* USER CODE BEGIN DAC1_Init 2 */

 /* USER CODE END DAC1_Init 2 */

}

 

The second case concerns IWDG, which generates the string "__HAL_RCC_IWDG_CLK_ENABLE()" which

obviously causes compilation to fail. I solved it by adding " #ifdef BUG_CLK_IWDG "

/**
 * @brief IWDG Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_IWDG_Init(void)
{

 /* USER CODE BEGIN IWDG_Init 0 */
#ifdef BUG_CLK_IWDG
 /* USER CODE END IWDG_Init 0 */

 /* Peripheral clock enable */
 __HAL_RCC_IWDG_CLK_ENABLE();

 /* USER CODE BEGIN IWDG_Init 1 */
#endif
 /* USER CODE END IWDG_Init 1 */
 LL_IWDG_Enable(IWDG);
 LL_IWDG_EnableWriteAccess(IWDG);
 LL_IWDG_SetPrescaler(IWDG, LL_IWDG_PRESCALER_8);
 LL_IWDG_SetReloadCounter(IWDG, 4095);
 while (LL_IWDG_IsReady(IWDG) != 1)
 {
 }

 LL_IWDG_ReloadCounter(IWDG);
 /* USER CODE BEGIN IWDG_Init 2 */

 /* USER CODE END IWDG_Init 2 */

}

 

ST Technical Moderator
November 17, 2025

Hello @Andrew Neil @cb.7 @SPozz.1 ,

 

Those issues are fixed, I suggest that you use the last STM32CubeMX version.

How to get STM32CubeMX 6.16.0:

  • Under this link .

  • Or update your current installation of STM32CubeMX using: Help > Check for Updates

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

ST Technical Moderator
July 16, 2025

Hello @cb.7 

 

First let me thank you for posting.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
July 16, 2025

Hello @cb.7 ,

 

Thank you for bringing these issues to our attention.

Related to the first problem (DAC Peripheral), an internal ticket is raised to the dedicated team

( Ticket Number : 214226 ).

Related to the second problem (IWDG Peripheral), an internal ticket is raised to the dedicated team

( Ticket Number : 214196 ).

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
November 11, 2025

@Mahmoud Ben Romdhane wrote:

Related to the second problem (IWDG Peripheral), an internal ticket is raised to the dedicated team

( Ticket Number : 214196 ).


See also: STM32U031C6 undefined reference to __HAL_RCC_IWDG_CLK_ENABLE().

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
SPozz.1
Associate II
July 19, 2025

Hello Mahmoud,
a third case came up:

immagine.png

static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* Peripheral clock enable */
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_CRC);

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 LL_CRC_SetInputDataReverseMode(CRC, CRC_INPUTDATA_INVERSION_BIT_BYBYTE);
 LL_CRC_SetOutputDataReverseMode(CRC, CRC_OUTPUTDATA_INVERSION_BIT);
 LL_CRC_SetInitialData(CRC, 0xFFFF);
 LL_CRC_SetPolynomialCoef(CRC, 32773);
 LL_CRC_SetPolynomialSize(CRC, LL_CRC_POLYLENGTH_16B);
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}


workaround added in main.c

/* USER CODE BEGIN CRC_Init 0 */
#define CRC_INPUTDATA_INVERSION_BIT_BYBYTE LL_CRC_INDATA_REVERSE_BIT_BYBYTE
#define CRC_OUTPUTDATA_INVERSION_BIT LL_CRC_OUTDATA_REVERSE_BIT
/* USER CODE END CRC_Init 0 */


Best regards,
Stefano

ST Technical Moderator
July 21, 2025

Hello @SPozz.1 

 

Let me thank you for posting and bringing this issue to our attention.

It has been escalated to the relevant team for fixing (Internal ticket number: 214506 Internal ticket number is only for reference, not accessible or usable outside of ST).

 

Best Regards.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
November 17, 2025

Hello @Andrew Neil @cb.7 @SPozz.1 ,

 

Those issues are fixed, I suggest that you use the last STM32CubeMX version.

How to get STM32CubeMX 6.16.0:

  • Under this link .

  • Or update your current installation of STM32CubeMX using: Help > Check for Updates

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.