Skip to main content
Jeanne Joly
Associate
Nov 5, 2020 9:46 AM UTC
Question

[Tutorial videos in STM32CubeMX] Your ideas are welcome

Around 40 tutorial videos are accessible from STM32CubeMX in Help menu/Tutorial videos since STM32CubeMX 6.0.0 release.

All those videos intend to answer frequent STM32CubeMX users questions.

It deals with various subjects such as FreeRTOS, DMA, GPIO, Software packs, System view tips, Getting started with X-Cube BLE, pinout view tips…

Those videos will be available to China users in the next STM32CubeMX release (6.1.0).

If you think that some specific tips, features or complex subjects are not yet addressed with these tutorial videos, we will be glad to hear your valuable proposals.

Thanks to share your ideas with maximum of details.

This topic has been closed for replies.

67 replies

martincho
Associate II
Mar 26, 2021 6:52 PM UTC

No music please.

Yes, one can mute the videos, of course. Here's the problem: How do we know someone will start talking in the middle of the video while it is muted?

That aside, ST does a fantastic job of having tons of video material to help designers. I love it.

dungeonlords789
Associate III
Apr 8, 2021 5:21 PM UTC

At this moment all STM32Cube_FW_WB_V1.11.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HealthThermometer\STM32CubeIDE is not fully compabiality with CubeMX. ST engineers use CubeMX for generate this projects and change a lot of. So this examples are blackbox.

Users need video tutorials how create BLE projects via CubeMX. For me the most interesting is BLE mesh projects: BLE_MeshLightingPRFNode, BLE_MeshLightingPRFNode, BLE_MeshLightingProvisioner.

@Jeanne Joly_O​ 

magene
Senior
May 8, 2021 8:04 PM UTC

I'd appreciate a step by step video that shows how to build a simple application from the bottom up that uses several peripherals that are typically used together (UARTs, USARTs, I2C, SPI, timer, SDMMC with FatFs). By bottom up, I mean starting with a new, empty STM32 project and adding the necessary .h and .c files into the project in a reasonably flat hierarchy. Here's an example of why this would be useful to non-master programmers like me. I have been able to get FatFs projects working when I start from the ST provided examples. But trying to figure out how that ST example works, like figuring out which SDMMC pins are being used, is exceptionally time consuming. And to make matters worse, integrating a working UART example into the working SDMMC/FatFS example breaks things that work fine in my stand alone examples.

dungeonlords789
Associate III
May 9, 2021 7:47 AM UTC

FatFS tutorial is needest!

AThom.3
Associate
May 23, 2021 7:09 AM UTC

A video on how to protect IP on devices, in particular the cheaper variants such as STM32F0 and STMF32F1 rather than the STM32F4's

dungeonlords789
Associate III
Jun 14, 2021 10:37 AM UTC
LMI2
Senior III
Jun 13, 2021 4:49 PM UTC

How to import your CubeMX project to Mbed.

dungeonlords789
Associate III
Jun 14, 2021 10:18 AM UTC

Just use FreeRTOS. It is very userfriendly.

LMI2
Senior III
Jun 18, 2021 8:11 PM UTC

Mbed users have written many libraries for various peripheral chips. Are there any for FreeRtos?

LMI2
Senior III
Jun 13, 2021 4:59 PM UTC

How to use SPI bus with MAX31865, PT100

How to use I2C bus with ADS1115, ADC

How to use I2C bus with DS3231, RTC

And other chips

dungeonlords789
Associate III
Jun 14, 2021 10:19 AM UTC

DS3231? Is it a joke?

This is chip from 2005. Use RTC build-in stm32.

LMI2
Senior III
Jun 16, 2021 9:59 AM UTC

I read some time ago that the RTC in STM32 was tricky to use. DS3231 is accurate and relatively easy to use. Besides, DS3231 is supported elsewhere, but not in STM32.

LMI2
Senior III
Jun 13, 2021 5:00 PM UTC

How to setup and build Ethernet HW and SW for various CPUs.

Grant Bt
Associate III
Jul 13, 2021 11:03 PM UTC

I would start by having the presenter not read the text from the PDF file. If the presenter is not explaining in better terms than the PDF then what is the point? I'm currently watching a video of someone reading the PDF.

https://youtu.be/U2alCU6pDjc?t=48

AndreasPA
Associate III
Jul 13, 2021 11:10 PM UTC

More hands on videos with the stm32MP1, currently some of the startup material doesnt run smoothly or you have to make little changes to the commands etc etc.

otherwise really we're better off going to something like begalbone. if it's a pain in the **** to get started with it and support is waiting a few weeks to get a response i dont see a reason to learn the system.

dungeonlords789
Associate III
Jul 14, 2021 6:03 PM UTC

stm32MP1 is very interesting! I am also interesting to find low-cost display with touch for stm32MP1. I need display 15" or more. Small example

PGogt
Associate II
Jul 16, 2021 10:32 AM UTC

Tutorials on Zigbee. A lot of the projects provided for Zigbee are black boxes. Would love to see an explanation on setting up a Zigbee project with FreeRTOS

dungeonlords789
Associate III
Jul 16, 2021 3:40 PM UTC

BLE is the best. Zigbee less interesting, less devices support it.

See examples \STM32CubeIDE_1.1.0\Repository\STM32Cube_FW_WB_V1.11.1\Projects