Skip to main content
Mikhail Sementsov
Associate
Sep 19, 2017 10:46 PM UTC
Question

Troubles with RCC in STM32CubeMX

Posted on September 20, 2017 at 00:46

Hi!

I found couple of troubles while programming STM32F030F4 with STM32CubeMX.

1. I used simple code like

while(1)

{ 

   HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_3);

   HAL_Delay(1);

}

which must generate 500 Hz square wave on PA3. It is actually work for 

STM32CubeMX V. 4.18.0, but 4.22.1 version gives 250 Hz signal.

2. I tried to use PLLCLK source (with the same code), but it absolutely doesnt work with any settings in V. 4.18.0 and      V. 4.22.1 - there is no signal, just little ripples on PA3. With HSE and HSI sources without PLL it works. Some months ago I used V. 4.20.1 without this trouble. Can you provide

a download link to

this version?

#pll #cubemx #stm32f0 #rcc
This topic has been closed for replies.

3 replies

ST Technical Moderator
Sep 20, 2017 8:25 AM UTC
Posted on September 20, 2017 at 10:25

Hi

Sementsov.Mikhail

,

Could you please share your .ioc file for more check your case?

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Mikhail Sementsov
Associate
Sep 20, 2017 4:26 PM UTC
Posted on September 20, 2017 at 18:26

https://drive.google.com/file/d/0B4JbVdnsjGUKNmFHaEtYdk5zVDQ/view?usp=sharing

There is three KEIL uVision V5.20.0.0 projects (description in README.txt) including .ioc files.

Jeanne Joly
Associate
Feb 6, 2018 12:50 PM UTC
Posted on February 06, 2018 at 13:50

Hi

Sementsov.Mikhail

Sorry for the late answer.

I was trying to reproduce your LED toggling issue on top of CubeMX4. I was using a F4 nucleo board but the LED toggle at 500Hz when the HCLK is set to 1ms.

No issue on that point. Do you still have this issue on the latest CubeMX release?

Regarding your second point, I suppose that you mean that the System Clock mux was configured with PLLCLK. I can't see any issue as well. If there is still an issue, are you sure that your clock is correctly configured (PLLCLK, HCLK, HSI...)?

BR. Jeanne