Skip to main content
Associate III
June 9, 2025
Question

TouchGFX and USBPD

Hello. 

 

I am trying to create a project that uses both the Nucleo GFX01M2 and SNK1M1 with the G071RB dev board. I want to configure my setup as a USB sink device. However, in STM32CubeMX I can select either the sink USBPD application, or the Touchgfx graphics application, but not both. What would be the best way to develop an application that utilizes both USBPD and TouchGFX? 

 

Thank you. 

This topic has been closed for replies.

8 replies

Soren Myllerup MIKKELSEN
ST Employee
June 16, 2025

Hello @TS-LMG 
I would recommend you to have a look at the STM32H7S78-DK example below. 

This demo shows USB DRD and DRP and UCPD: https://www.youtube.com/watch?v=FpX9AdRocYQ

And its available as FS: https://www.st.com/en/microcontrollers-microprocessors/stm32h7r3-7s3.html# 

Hope it helps you move forward.

 

Best regards

Soren Mikkelsen

TS-LMGAuthor
Associate III
June 16, 2025

Hello @Soren Myllerup MIKKELSEN,

I will look into using the STM32H7S78-DK for proof of concept purposes. However, the IC itself is quite expensive for my application. I would look to downgrading it in the future. Do you know where I can find the example show in the video? 

Thank you.  

TS-LMGAuthor
Associate III
June 16, 2025

@Soren Myllerup MIKKELSEN 

 

For the STM32H7S78-DK, I noticed that I cannot select both TouchGFX and Sink USBPD application in the software packs selector from within cubeMX. How can I merge TouchGFX and USBPD? 

Soren Myllerup MIKKELSEN
ST Employee
June 17, 2025

@TS-LMG 
The demo source is available here: https://www.st.com/en/microcontrollers-microprocessors/stm32h7r3-7s3.html#tools-software Under "Demo resources"

For the TouchGFX and USBPD application combination from scratch, i will ask a colleague to answer on the thread here. 

Are you only looking for MCU to drive USB application? 

TS-LMGAuthor
Associate III
June 17, 2025

Hello @Soren Myllerup MIKKELSEN,

I found the demo source and looked at the source code. By the sounds of it, I will have to manually merge TouchGFX and USBPD together. I noticed the demo has no IOC file. 

 

I am looking for an MCU that can do USBPD and drive a TFT display at the same time, as my application required PD negotiation and some kind of graphical interface. 

 

Regards,

Tom

Soren Myllerup MIKKELSEN
ST Employee
June 18, 2025

Hello @TS-LMG 
One will shortly answer you on the merge of these 2. 

The example shows this setup (TouchGFX app + UCPD). 

What kind of display do you want to run? the STM32H7R3 comes in LQFP144 wiht UCDP and 1xQuadSPI NOR flash if, You could then connect a parallel or SPI display. 

 

Best regards

Soren Mikkelsen

TS-LMGAuthor
Associate III
June 18, 2025

Hello @Soren Myllerup MIKKELSEN,

 

I do have the GFX01M2 nucleo. I think the size of this TFT display is ideal for my application, although not set in stone. I purchased the STM32H7S78-DK as it has working examples. 

 

GaetanGodart
ST Employee
June 23, 2025

Hello @TS-LMG ,

 

I was able to enable both TouchGFX and USBPD for an STM32H7S7 board in STM32CubeMX:

GaetanGodart_0-1750669720265.png

(I first enabled TouchGFX, then CRC, then USBPD if that helps)
Note that it is pink because I did not configure everything correctly.

 

What versions are you using?
Can you share your project?

 

You could manually merge the files for the USBPD to a project with TouchGFX enabled by creating both project and then using a file/folder comparator to see what is missing but that would be quite some work.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)