Skip to main content
Robmar
Senior II
Nov 8, 2022 6:17 PM UTC
Question

ToolChain Manager is throwing a Network error "Failed to fetch the toolchain list, please check your network settings." PC is connected, it loaded updates for four of the tools, resetting the IDE each time. Anyone had this issue?

I also see this build error: make: *** [makefile:109: default.size.stdout] Error 1 your_project C/C++ Problem

This topic has been closed for replies.

9 replies

Semer CHERNI
ST Employee
Nov 9, 2022 9:43 AM UTC

Hello @Robmar​ 

First let me thank you for posting.

Could you please provide more details about the error message:

  • Some screenshots would be helpful
  • The build log
  • Are you using a proxy?

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Robmar
RobmarAuthor
Senior II
Nov 9, 2022 11:42 AM UTC
Hi Semer,
Thanks for your reply.   The new project I made compiled perfectly and
ran in debug until I imported McHF, where on opening the ToolChain
Manager, it said to update 4 of the entries, which I did, the last one
failed, and now I get a network error, but my PC is connected to the
internet. Here is the screen shot:
Tesla DeLorean
Guru
Nov 9, 2022 9:49 AM UTC

Check things like firewalls and AV which might interfere with normal operation.

Perhaps reinstall, or Run As Administrator.

Check with IT​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Robmar
RobmarAuthor
Senior II
Nov 9, 2022 11:50 AM UTC

Thanks but my Internet connection works fine, the IDE even uploaded the updates for 4 tool chain items without problem. If I delete all the items will it rebuild the toolchain for the project?

Julien D
ST Employee
Nov 9, 2022 12:28 PM UTC

Looking at the screenshot you're falling in a known bug in the Toolchain Manager.

When all listed toolchains are already installed the fetch ends with an error. It can be safely ignored while waiting for a fix.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Robmar
RobmarAuthor
Senior II
Nov 9, 2022 12:35 PM UTC

hey thanks, I hope it's that!

My other problem is installing DSP for CMSIS, its missing from the repository for some reason.

Julien D
ST Employee
Nov 9, 2022 12:50 PM UTC

For that I add STM32CubeMX topic to put this thread on the radar of more knowledgeable peoples.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.