Skip to main content
Associate III
July 15, 2025
Question

To bypass an external waveform

Hello.

I'm using a NUCLEO-311RE board.

I'm looking for a way to bypass the external waveform as it is.

This is my timer setting

giwonKIM_0-1752622787998.png

 
static void MX_TIM1_Init(void)

{



/* USER CODE BEGIN TIM1_Init 0 */



/* USER CODE END TIM1_Init 0 */



TIM_SlaveConfigTypeDef sSlaveConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};

TIM_OC_InitTypeDef sConfigOC = {0};

TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};



/* USER CODE BEGIN TIM1_Init 1 */



/* USER CODE END TIM1_Init 1 */

htim1.Instance = TIM1;

htim1.Init.Prescaler = 0;

htim1.Init.CounterMode = TIM_COUNTERMODE_UP;

htim1.Init.Period = 1;

htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim1.Init.RepetitionCounter = 0;

htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

if (HAL_TIM_Base_Init(&htim1) != HAL_OK)

{

Error_Handler();

}

if (HAL_TIM_OC_Init(&htim1) != HAL_OK)

{

Error_Handler();

}

sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;

sSlaveConfig.InputTrigger = TIM_TS_ETRF;

sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;

sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;

sSlaveConfig.TriggerFilter = 0;

if (HAL_TIM_SlaveConfigSynchro(&htim1, &sSlaveConfig) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

sConfigOC.OCMode = TIM_OCMODE_TOGGLE;

sConfigOC.Pulse = 0;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;

sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;

if (HAL_TIM_OC_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)

{

Error_Handler();

}

sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;

sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;

sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;

sBreakDeadTimeConfig.DeadTime = 0;

sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;

sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;

sBreakDeadTimeConfig.BreakFilter = 0;

sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;

sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;

sBreakDeadTimeConfig.Break2Filter = 0;

sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;

if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN TIM1_Init 2 */



/* USER CODE END TIM1_Init 2 */

HAL_TIM_MspPostInit(&htim1);



}

 

In this way, a waveform with a frequency of 1/4 of the external waveform is generated. Is there another way to copy the external waveform as it is?


Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

2 replies

TDK
July 16, 2025

> NUCLEO-311RE

There is no such board. Maybe NUCLEO-F411RE?

 

> Is there another way to copy the external waveform as it is?

Use a buffer amp or op-amp in follower configuration.

Can't have a channel output from a timer be the same as the input clock.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
July 16, 2025

@giwonKIM wrote:

Is there another way to copy the external waveform as it is?


As @TDK said, no - but why do you want to do that?

If you say what you're actually trying to achieve, people may be able to offer other suggestions ...

http://www.catb.org/~esr/faqs/smart-questions.html#goal

https://xyproblem.info/

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.