Skip to main content
yafisdamda
Associate III
Nov 30, 2015 8:52 AM UTC
Question

TIM3 problem in stm32 cube HAL library

Posted on November 30, 2015 at 09:52

Hello.

I am using STM32F0xx with stm32cube lib as the dev platform. 

My application requires TIM3 peripheral. I am using __HAL_TIM_SET_COUNTER to set the cnt value at runtime. I need the timer count value for some calculation and i re-set it using the above macro every fixed interval. What i am observing is when set the counter value, stop the timer and restart it. It doesnt report interrupts. 

What is the correct procedure to set the counter value while the timer is running??

#stm32-cubemx-tim-interrupt
This topic has been closed for replies.

2 replies

matic
Associate III
Nov 30, 2015 10:10 PM UTC
Posted on November 30, 2015 at 23:10

I don't understand why would you like to set CNT register manually? To which value?

Tesla DeLorean
Guru
Dec 1, 2015 12:30 AM UTC
Posted on December 01, 2015 at 01:30

I generally prefer to read two successive values and compute a delta between them, rather than reset or change the counter asynchronously.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..