Skip to main content
Blacbird
Associate II
Mar 25, 2019 3:44 PM UTC
Solved

TIM3 as Timebase Source on STM32F302RB

I recently switched an older project to CubeMX 5.1.0 and the F3 firmware package V1.10.0. We used freeRTOS and tim3 as the timebase source as tim1 and tim2 are already in use. The program does not pass the initial timebase configuration any more and the call of HAL_TIM_IRQHandler(&htim3) in the TIM3_IRQHandler(void) has disappeared. When using any other timer the call is generated and it works if I manually add it in the user code section, could it be that this is a bug in the code generation?

This topic has been closed for replies.
Nesrine.JLASSI
Nesrine.JLASSIBest answer
Visitor II
Apr 29, 2019 4:04 PM UTC

Hi @Blacbird​ 

Thanks for the feedback, please try the issue with STM32CubeMX version 5.2.0. The problem is solved.

(Your attention please: in your .ioc file, you have used TIM4 as timebase source not TIM3 ).

Best regards,

Nesrine.

4 replies

Nesrine.JLASSI
Visitor II
Mar 27, 2019 3:15 PM UTC

Hi @Blacbird​ 

Could you please send me your .ioc file to check the problem.

Best regards,

Nesrine

Blacbird
BlacbirdAuthor
Associate II
Apr 25, 2019 9:29 AM UTC

Hi @Nesrine.JLASSI​,

I appended the .ioc file. Sorry that it took that long for me to answer, I forgot that I disabled the notifications.

best wishes,

Tobias

Nesrine.JLASSI
Nesrine.JLASSIBest answer
Visitor II
Apr 29, 2019 4:04 PM UTC

Hi @Blacbird​ 

Thanks for the feedback, please try the issue with STM32CubeMX version 5.2.0. The problem is solved.

(Your attention please: in your .ioc file, you have used TIM4 as timebase source not TIM3 ).

Best regards,

Nesrine.

Blacbird
BlacbirdAuthor
Associate II
Apr 30, 2019 8:24 AM UTC

Hi @Nesrine.JLASSI​ ,

thank you for your answer! The issue was indeed fixed with the last cubeMX version. We used TIM4 in the .ioc to evade the problem and keep on developping.

best wishes,

Tobias